Caterpillar Marine offers a complete line of U.S. EPA Tier 4 and IMO Tier III Cat® C280 engines.

Hamburg, Germany - Caterpillar Marine is now offering Cat® C280 medium-speed diesel engines for U.S. Environmental Protection Agency (EPA) Tier 4 and International Maritime Organization (IMO) Tier III service.   The EPA Tier 4 standards applied to all new U.S. flagged vessels starting in January 2014 and IMO III standards will apply to all new vessels entering IMO NOx Emissions Control Areas (NECA) starting in January 2016.

The C280 engines are available in eight, 12 and 16-cylinder models spanning a power range from 2300 ˗ 5060 kW as main engines – conventional and diesel electric – and also as auxiliary generator sets. The latest models offer significant benefits over earlier units. As well as reduced emissions, they consume less fuel and have lower through-life owning and operating costs.

Over three decades of continuous development, the C280 engine series has clocked up more than 45 million operating hours. Its reliability and durability has found particular favor among operators of offshore supply vessels, coastal cargo ships, tugs, fishing vessels, inland waterway craft and work boats. All engines in the C280 range are now available worldwide through the Cat dealer network which provides comprehensive support through the life cycle of the solution and continuous customer care.

Nathan Kelly, Caterpillar Marine production definition engineer, says the introduction of the Tier 4 engine range is an important milestone because customers can now benefit from the latest NOx emission technology based on selective catalytic reduction (SCR). The choice of SCR over other NOx reducing technologies, Kelly explains, was made based on the Caterpillar commitment to customers to offer solutions that provide the highest uptime and minimize overall total lifecycle cost. Furthermore, he says, an independent study undertaken by the International Council on Clean Transportation published in March 2014, highlights the benefits of emissions reduction technology and the wide range of companies that have adopted SCR as the most efficient solution for the marine industry.

“SCR was a clear choice for us,” explains Kelly. “We have more than 160,000 Tier 4 Final and Interim engines in land-based operations using various NOx-reduction technologies. In marine applications, we specifically chose the best technology to fit the needs of our industry.  We view SCR as the preferred option for the commercial marine industry. ” 

Outlining the key benefits, Kelly explains: “The C280 is already renowned for its high uptime, reliability and durability, but for these Tier 4 engines our priority was to achieve the lowest lifecycle owning and operating cost. We have succeeded in this by improving engine fuel efficiency. Unlike previous emissions Tiers, our Tier 4 engines can run at optimal fuel efficiency because the SCR system is in place to reduce the higher NOx output. Any concerns about Diesel Exhaust Fluid (DEF) cost are more than offset by the improved fuel efficiency as a result of utilizing the SCR technology.”

Ensuring maximum operating safety at all times is crucial, Kelly adds. “Unlike some other NOx reduction technologies, our engines operate without interruption even in the event of SCR failure or running out of DEF. There is no effect to engine operation.”

Cat marine power and propulsion solutions are backed by the worldwide Cat dealer network with trained technicians to ensure service support is never out of reach. For more information on Caterpillar Marine, visit www.cat.com/marine. For information on Cat Propulsion products, visit www.catpropulsion.com. Follow us on Facebook: www.facebook.com/caterpillarmarine and Twitter @catmarineglobal.

# # #

About Caterpillar Marine

Caterpillar Marine, with headquarters in Hamburg, Germany, groups all the marketing and service activities for Cat and MaK™ marine diesel, dual fuel and gas power and propulsion systems within Caterpillar Inc. The organisation provides premier power solutions in the medium- and high-speed segments with outputs from 93 to 16,800 kW in main propulsion and 10 to 16,100 kWe in marine generator sets as well as a comprehensive portfolio of propulsion solutions. The sales and service network includes more than 2,100 dealer locations world-wide dedicated to support customers in ocean-going, commercial marine and pleasure craft wherever they are.

More information is available at: MARINE.CAT.COM/pr

About Caterpillar

For nearly 90 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent. Customers turn to Caterpillar to help them develop infrastructure, energy and natural resource assets. With 2014 sales and revenues of $55.184 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. The company principally operates through its three product segments - Resource Industries, Construction Industries and Energy & Transportation - and also provides financing and related services through its Financial Products segment. For more information, visit caterpillar.com. To connect with us on social media, visit caterpillar.com/social-media.

More information is available at www.cat.com.

Press Inquiries

Jenna Janik Marcoux                                            
Phone: +1 713 895 1449
Marcoux_Jenna_J@cat.com