New Mobile, Diesel Generator Set Rated for 182 kW Expands Caterpillar’s Tier 4 Final Offerings

For Worldwide Release: March 25, 2019
Release Number: EEPR0419

DEERFIELD, IL – Caterpillar Inc. today introduced the Cat® XQ230, a 60 Hz mobile diesel generator set rated at 182 kW (227.5 kVA) meeting Tier 4 Final emission standards for prime operation set by the U.S. Environmental Protection Agency. Eleven percent smaller than the previous model, the Cat XQ230 generator set delivers additional power in a smaller footprint.

The Cat XQ230 generator set has been engineered to operate at lower noise levels than competitive packages. This generator set is equipped with rental-ready features including heaters, a battery charger and a permanent magnet generator (PMG). An optional 600V generator is available, giving the operator ultimate flexibility with a single generator set capable of producing power at 600V, 480V, 240V and 208V. Caterpillar’s diesel particulate filter (DPF) regeneration strategy ensures seamless operation even at low loads or in cold weather without the need to add additional components, cost or complexity. Regeneration is transparent to the operator and the unit does not need to be taken offline.

The Cat XQ230 is equipped with the standard EMCP 4.2B control panel. A user-friendly interface allows for engine and generator monitoring and control. Automatic paralleling controls are available with the optional EMCP 4.4. In addition, Cat® Connect technology is available to track and manage the machine remotely by collecting data and reporting on asset performance, run hours, fuel consumption, maintenance needs, and other statistics. This timely information allows customers to better control costs, improve performance and reduce risks.

“The new Cat XQ230 generator set joins a lineup of Tier 4 Final mobile diesel generators sets delivering power from 28 kW (35 kVA) to 455 kW (568 kVA),” said Gareth Osborne, productdefinition manager, Caterpillar Electric Power. “Caterpillar’s complete lineup of mobile electric power solutions delivers robust, durable products with a range of rental-ready features to meet job requirements and applications anywhere in the world.”

The Cat XQ230 generator set complies with Canadian Standards Association (CSA) requirements, as well as Transport Canada (UN31A) requirements.

For more information, visit the online Cat® Rental Store or email cat_power@cat.com

Available Images

Download here or contact Erin Collins at ecollins@gelia.com

Cat® XQ230 mobile diesel generator set Cat® XQ230 mobile diesel generator set
Cat® XQ230 mobile diesel generator set

# # #

 

About Caterpillar

For more than 90 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent. Customers turn to Caterpillar to help them develop infrastructure, energy and natural resource assets. With 2018 sales and revenues of $54.722 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. The company principally operates through its three primary segments - Construction Industries, Resource Industries and Energy & Transportation - and also provides financing and related services through its Financial Products segment. For more information, visit caterpillar.com. To connect with us on social media, visit caterpillar.com/social-media.

 

CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

©2019 Caterpillar
All Rights Reserved

 

Press Inquirie
 

Erin Collins
Gelia
Tel: +1 716-629-3176
ecollins@gelia.com    

Rachel Perva
Caterpillar Inc.
Tel: +1 309-675-7267
perva_rachel@cat.com

 

Reader Responses

Caterpillar Inc.
Electric Power Division
P.O. Box 0610
Mossville, IL 61552-0610