Caterpillar Introduces New Cat® Locator Device for Machine Attachments and Jobsite Assets

For Worldwide Release: February 2019
Release Number: 64PR19

Caterpillar is pleased to announce the addition of the PL161 attachment locator to the Locator series of the Cat® Product Link™ hardware product line. The PL161 locator is the most advanced OEM integrated technology solution for attachment tracking. With the ability to track location and utilization, users can know where their attachments are across all worksites, reduce the number of lost attachments, and plan for attachment maintenance and replacement.

The PL161 attachment locator can be used on attachments and non-powered assets as an affordable option for last known location tracking, and it integrates easily into users’ operation for full fleet management of machines and attachments from one dashboard on a smartphone or a tablet.

The PL161 locator is a customer installable device that supports operation in harsh environments. The compact design of the locator makes it compatible for a wide range of assets without interfering with the work they are doing. Bluetooth range is up to 30 meters (100 feet), depending on the environment and any obstructions. The device is battery powered with an estimated life of 2 years.

The PL161 locator is designed to be used with the Cat App and with other PL Series scanning devices installed on Next Generation excavators and retrofit kits are available for older machines. When using the Cat App within range of the PL161 locator device, the location will be logged automatically. This system leverages cellular and Wi-Fi connectivity through the user’s own smartphone or tablet to transmit data to the VisionLink® and My.Cat.com applications. Purchase of the PL161 locator comes with a subscription to VisionLink for the life of the device.

PL161 locator is available from the factory on select attachments and will be factory-installed on all excavator attachments starting from the middle of 2019. The Cat App is compatible with most smart devices that have Bluetooth 4.0 or later and is available for download from the App Store (iOS) or Google Play Store (Android). 

 

Specifications

Dimensions cm (in)

Approximately 5 x 3.8 x 1.5

(2" x 1.5" x 0.6")

Weight, grams (oz)

85 (3.0)

# # #

 

Note to Editors: Caterpillar rolls out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.

CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

VisionLink is a trademark of Trimble Navigation Limited, registered in the United States and in other countries.

©2019 Caterpillar. All Rights Reserved.

Press Inquiries

Caterpillar Trade Press Media Representatives

Americas

Sharon Holling: Holling_Sharon_L@cat.com

Johanna Kelly: Kelly_Johanna_L@cat.com

Europe, Africa, Middle East

Francine Shore: Shore_Francine_M@cat.com

Reader Requests
www.cat.com/requestCatinfo