Peabody orders complete Cat® longwall with advanced automation for North Goonyella Mine

For Worldwide Release: March 2018 
Release Number: 155PR18

Peabody recently ordered a complete Cat® longwall mining system for its North Goonyella Mine located in central Queensland, Australia. The Cat longwall system includes roof supports and a face conveyor for a 300-meter face, shearer and beam stage loader. The system features advanced longwall automation technology to enhance safety and production.

Delivery of the system is planned for the second quarter of 2019. The regional Cat dealer, Hastings Deering, will provide technical support for installation and commissioning of the longwall and will provide operational support going forward.

North Goonyella produces premium coking coal via a Cat longwall system, which was instrumental in achieving record production from the mine in 2017. The decision to move to a new Cat system was driven by technological advances that enable automated shearer steering and face alignment, reduced exposure of operators to dust, and less maintenance.

Longwall automation

The Cat EL3000 shearer for North Goonyella will be equipped with the proven Cat PMC™ Evo-S control system, intelligent software modules and advanced measuring technology. The automation package enables the shearer to be operated by a single operator using remote control. This package includes automation logic to minimize overload situations and diagnostic tools to maximize uptime.

Software tools and sensors in the gate ends and in the shield controllers enable advanced calculations for full 3D navigation and an accurate floor profile calculation. In total, the Cat automation package enhances safety and allows improved use of manpower, reduces coal dilution, enables faster haulage speeds, improves face management and increases life of all longwall equipment, including the face conveyor and roof supports.

Caterpillar will supply an efficient dust suppression system, designed using a holistic approach to mitigating operator dust exposure levels. With thorough understanding of dust generation processes in longwall operations and details defining the operating environment, Caterpillar engineers will design a state-of-the-art dust suppression system for North Goonyella.

Additionally, Caterpillar has developed a corrosion protection strategy to improve resistance to corrosion and to minimize maintenance activities in the North Goonyella mine environment. For example, the 153 new Cat roof supports will have specially coated rods used in the hydraulic legs, and susceptible components will be built from highly corrosion resistant materials.

For more information about Cat underground mining systems, contact the regional Cat dealer or go to: Cat.com/Mining

# # #

Note to Editors: Caterpillar rolls out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.

CAT, CATERPILLAR, their respective logos, “Caterpillar Yellow” and the “Power Edge” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

©2018 Caterpillar All Rights Reserved

 

alt alt