Cat® Command remote-control
Cat® Command remote-control

Caterpillar expands Cat® Command remote-control operation to excavator line, enhancing safe machine operation

 

For Release in North America and Japan: August 2021
Release Number: 471PR21

New Cat® Command for Excavating provides remote-control operation for select Cat excavators. Removing the operator from the machine in potentially hazardous operating environments, Command for Excavating enhances safe machine operation, while reducing operator fatigue to increase productivity. Six Cat excavators spanning the 20 to 40 metric ton class sizes – Cat 320, 323, 326, 330, 336 and 340 models – can now be equipped with either line-of-sight or non-line-of-sight remote operating configurations.

Cat excavators are made Command-ready through a dealer-installed field kit for new or existing fleet machines. Providing excellent visibility, the kit features multiple cameras for non-line-of-site operation from the Command station that offer a view of the area surrounding the machine plus the ability to stream on-site video feeds. Alongside the cameras, indicator lights, microphone, wireless receiver, and antenna are all mounted on top of the cab to minimize the risk of damage.

Deeply integrated with the excavator’s electronics, Command controls allow users to experience the same machine response as if they were operating from inside the cab, allowing a high level of productivity to be maintained from a safe distance. Machine technology features such as Grade Assist, Swing Assist and E-Fence can also be set, activated and deactivated remotely without the need to be set manually from inside the cab. Excavators are efficiently switched between remote and manual operation via a ground-level switch.

With users comfortably controlling dig, lift and tracking functions from a safe location, Command for Excavating enables production to restart immediately following disruptive processes, such as blasting in quarry applications. It also enhances safety and improves machine productivity on a range of projects like operating in unstable underfoot conditions, brownfields, shore work, demolition and site decommissioning, and stevedoring.

Flexible, precise control

Command for Excavating offers a solution to workforce shortages by opening opportunities to those with physical limitations that prevent them from climbing into the equipment, attracting a new generation of worker and increasing the longevity of experienced operators. Removing the operator from the cab also offers training advantages for newer operators.

The Command system includes two different remote operating options. Ideal for temporary or emergency remote operation with no on-site communications infrastructure required, the Command console offers line-of-site machine control through a lightweight, compact console, supported by a comfortable shoulder harness. Offering machine control from up to 437 yd (400 m) away, the console controls all excavator functions with virtually no response delay. Built-in safety features stop all excavator movements if the remote shutdown switch is pressed, wireless communication is lost, or the console is tilted more than 45 degrees from normal operating position.

The new Command station provides non-line-of-site operation from the comfort of an air-conditioned office on-site or many miles away, as distance is limited only by the capabilities of the wireless network. Reducing downtime for shift changes or the need to travel to the jobsite, operators can easily control up to five different machines at a single or different sites from one station.

Eliminating fatigue-inducing vibration of machine movements at the site, the customized Command station reflects the cab environment and positions users in a familiar, comfortable seated position that simulates traditional machine control. Station design includes joystick and foot pedal controls to operate all the company’s Command-ready equipment. Universal screen mounts positioned in front of the user provide easy view of the excavator’s camera displays, while touchscreen monitors similar to the in-cab display offers machine control.

More information about Cat Command for Excavating can be found by contacting the local Cat dealer or visiting: https://www.cat.com/commandforexcavating.

 

of

Cat® Command Console being used to remotely operator a Cat® 320 excavator on a hillside with loose gravel.

of

Cat® Command Stations in an office environment being used to remotely control excavators and wheel loaders at a river terminal to unload barges and ship cargo holds.

of

Cat® 320 excavator loading trucks by remote control on the edge of a hillside.

of

Cat® 320 excavator working in the cargo hold of a ship by remote control.

of

Cat® Command Console being used to remotely operator a Cat® 320 excavator on a hillside with loose gravel.

 

 

Product & Service News

See the latest product and engine announcements from Caterpillar.

See the Latest News

 

# # #

 

Note to Editors: Caterpillar rolls out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.

CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

©2021 Caterpillar All Rights Reserved 

 

 

Press Inquiries

Caterpillar Trade Press Media Representatives

Americas

Sharon Holling: Holling_Sharon_L@cat.com

Johanna Kelly: Kelly_Johanna_L@cat.com

Europe, Africa, Middle East

Francine Shore: Shore_Francine_M@cat.com

Reader Requests

www.cat.com/requestCatinfo