Cat® dragline bucket
Cat® dragline bucket

Innovative new Cat® dragline bucket boosts fill speed and increases payload

 

 

For Release Worldwide: February 2020
Release Number: 78PR20

The new Cat® double clip back bucket for draglines features an innovative design that increases fill speed and reduces bucket weight for faster cycle times and greater payload. The patented design also eliminates the high-maintenance spreader bar from the rigging system.

The wide mouth, aggressive lip angle, and low front height reduce drag power required to fill the bucket. The design minimizes the required fill distance for improved productivity and reduced bucket wear. The unique shape of the rear wall enables the bucket to fill without upper rear corner voids, and it increases material density in the bucket for optimum payloads on every pass. It also clearly shows the operator when the bucket is full and should exit the cut.

Eliminating the hoist rigging spreader bar has additional benefits, such as reduced wear and tear on the top rails and trunnions. Fewer system components result in less inventory management and reduced maintenance cost. The rigging system design also gives the operator better control of the bucket and reduces the opportunity for an inexperienced operator to damage it.

The unique trunnion design and location on the clipped portion of the bucket protects the lower hoist link from wear and provides quick dumping of the payload. The design includes a cast-in deflector to protect and increase the life of the trunnion.

The new Cat bucket is available for a wide range of dragline sizes and applications, no matter what the brand of machine. Using data-driven analysis, Caterpillar designs each bucket for the specific dragline and application.

The design process uses all significant parameters, including ground density, wear package, rigging package and bucket weight to optimize performance within the dragline’s rated suspended load. Reduced dead weight of the double clip back bucket, as compared to conventional designs, ranges from 2 to 10 percent depending on the application.

Cat dragline buckets also include wear packages based on the mine’s material abrasiveness and digging conditions. The Cat dragline bucket lip nose casting supports the Cat CapSure™ adapter and tooth system. The system delivers long wear life and hammerless installation of teeth for enhanced safety and faster removal and replacement.

For more information about Cat draglines, contact the local Cat dealer or go to: www.cat.com/mining

 

 

of

Cat double clip back dragline bucket, front quarter view

of

Cat double clip back dragline bucket, 67 cu m (88 cu yd)

Product & Service News

See the latest product and engine announcements from Caterpillar.

See the Latest News

 

 

# # #

 

Note to Editors: Caterpillar rolls out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.

CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

©2020 Caterpillar All Rights Reserved

 

Press Inquiries

Caterpillar Trade Press Media Representatives

Americas

Sharon Holling: Holling_Sharon_L@cat.com

Johanna Kelly: Kelly_Johanna_L@cat.com

Europe, Africa, Middle East

Francine Shore: Shore_Francine_M@cat.com

Reader Requests
www.cat.com/requestCatinfo