Altorfer Cat was the top-of-mind choice because of strong support they delivered to UnityPoint Health in the fall of 2013, when a tornado outbreak struck in the area. Those tornadoes brought significant power outages to the immediate community, including a prompt care facility on the UnityPoint health campus. Altorfer Cat quickly supplied a Cat® XQ175 rental generator set to serve as a standby power source.
Learn MoreMarpor Corporation’s Denny’s restaurants in Puerto Rico had enough Cat standby power to keep their power on through hurricane Maria and to help out their community by handing out 4,000 breakfasts to people in need.
Learn MoreA BETTER IDEA: We didn’t know when the power was going to come back on. Some people didn’t get power for up to three weeks.
Learn MoreA network of 19 Cat® diesel generator sets provided secure and safe power for every aspect of the festival venue.
Learn MoreIn addition to improved fuel efficiency, the next generation XGC1900 rental generator provides significant power density advantages. Caterpillar developed new exhaust stacks that reduce spacing requirements for sites requiring multiple units.
Learn MoreThe Cat XQ230 is powered by a C 7.1 Tier 4 Final compliant industrial diesel engine offering the perfect balance of durability, efficiency and low emissions. With advanced research and development techniques, the after treatment system is precisely matched to the engine ensuring performance is optimized for maximum productivity.
Learn MorePackaging 1100 kVA in a 20’ ISO transportable container, the power density offering in the XQP1100 is increased and paralleling controls with an Electrically Operated (EO) breaker are featured as standard equipment. The XQP1100 is a fully self-contained unit capable of running eight hours without refueling.
Learn More