Myanmar had one of the lowest electrification rates in the world and development increased demand. A major energy crisis left millions of residents without electricity. A high-quality and high-performance power plant was needed quickly. MSP Cat and Caterpillar delivered 13 Cat CG260 gas generator sets and additional installation components. The $46.5 million project was completed on time, and the 50 MW power plant is supporting the national power grid.
Learn MoreCabo Rojo Gas is wholesale supplier of gasoline, diesel fuel and propane to retail gas stations, fleets and other industrial customers throughout Puerto Rico. During hurricane season, emergency services, businesses, and residents have a need for an uninterrupted supply of fuel. To accommodate this need for critical backup power, they chose reliable, efficient Cat standby power at their five distribution centers to keep pumps working and their delivery trucks on the road.
Learn MoreTo minimize high operating costs from diesel fuel, SWN turned to Caterpillar Oil & Gas and Cat dealer Riggs Cat for a dual-fuel solution – Dynamic Gas Blending (DGB™).
Learn MoreTrillions of cubic feet of natural gas trapped beneath Fort Knox are now fueling Cat® generator sets, which provide prime and standby power for the base and – through a process known as combined heat and power – heat and cool the installation’s 400-bed hospital as well.
Learn MoreHeber Light & Power keeps the electricity flowing through a peak load shaving effort that includes nine gas generator sets from Caterpillar. Around the clock, analysts at Heber Light & Power examine hour-by-hour wholesale energy prices to determine the most cost-effective combination of potential power sources to meet demand at any given time.
Learn MoreWhen it is complete, Markham Centre will be a development of 30 million square feet including residential, commercial and institutional buildings, and home to over 41,000 residents and 39,000 employees. Whether the Cat fleet is providing emergency power to our customers, or grid power, or thermal energy for our heating system, high reliability is the goal for MDE and our suppliers.
Learn MoreThe cogeneration system was put into service in 2004 and since that time has been used to generate the power need to cover the basic load. The remaining energy demand continues to be met by the four conventional heating boilers. The Cat G3520C natural gas generator set meets the heating needs of about 2,100 households, and generates 16.5 million kilowatt hours of electricity per year. Most of that energy is fed into the local power grid and sold.
Learn MoreIn an effort to meet the Mtwara and Lindi regions' need for power, Artumas Group, Inc., designed a comprehensive gastopower project, tapping the abundant natural gas resources in the Mnazi Bay Concession. It took a cooperative effort between the local Cat® dealer and the installation and management team to ensure the successful commissioning of the power plant, notes Gathercole.
Learn MoreEnsuring power to an island community takes the commitment of a strong company and the most reliable equipment available. The C175-16 runs continuously, providing the island with 1.3 to 2 MW of power. The island’s peak power need of 3.3 MW is met with the addition of one of the 3516 generator sets.
Learn MoreChester, California prepared to undergo a 72-hour power shutdown so that Pacific Gas and Electric (PG&E) could replace power poles and their cross-arms. PG&E’s North Valley General Construction Line Division (GC Line) contracted the local authorized Cat® dealer to provide temporary power to the town during this shutdown.
Learn MoreThe power plant needed to meet the demands of a tropical location, and include a comprehensive Supervisory Control and Data Acquisition (SCADA) system to provide local and remote monitoring and control capabilities.
Learn MoreProvo Power needed help reducing smog and emissions for their Utah Valley community. Using Cat generator sets, they constructed a new plant to produce cleaner air for the city.
Learn MoreThe innovative approach by Henri Fraise Fils & Cie, Madagascar of owning power stations and selling the electricity also benefits JIRAMA. By providing additional power, JIRAMA is able to invest more time and resources in other electricity grid improvements throughout the country.
Learn MoreIn order to expand its power generation, IMEA Rantoul implemented a solar power project that generated remarkable results.
Learn MorePeople’s Electric Cooperative uses Cat® generator sets to provide efficient power to rural areas in south central Oklahoma at reasonable rates. PEC primarily runs the gensets when the cost of generating their own power is lower than purchasing grid power.
Learn MoreAs the population of Lehi, Utah grows, Lehi City Power needed a way to offset the high cost of power from the grid. With support from their Cat® dealer, Lehi developed a power generation facility featuring three Cat G3520H generator sets capable of producing nearly 10 percent of the power needs for 20,000 customers.
Learn MoreIn addition to cost savings for the city, the Cat® generator sets provide peak power production support and backup power in case of a citywide blackout. During power outages, city runs on gensets, the Cat 3516B diesel generators provide the ability to block load segments of the city's distribution system and then transition to the G3520C natural gas generator sets.
Learn MoreSEDCO engaged Caterpillar as the genset provider for its 5 MW natural gas-based power plants, primarily as a captive source of power exporting to grid. Two CAT® G3612 generator sets were chosen to power the project, based on the maximum uptime and ability of the engine to run continuously on field gas.
Learn MoreTo help overcome its growing challenges and provide power, Santa Clara turned to its local Cat® dealer, Ken Green of Wheeler Power Systems, headquartered in Salt Lake City. Wheeler Power Systems has been the authorized Caterpillar distributor for the state of Utah for 45 years, with responsibility for sales and product support in Utah, central eastern Nevada and southwest Wyoming.
Learn More