Caterpillar Launches CG170-B Series of Gas Generator Sets with Increased Efficiency, Reliability and Improved $/kW Performance

For Worldwide Release: January 16, 2019

Mannheim, Germany – Caterpillar Energy Solutions is pleased to introduce the CG 170B 50 Hz series of generator sets with increased power output from 1.3 – 2.3 MW, higher reliability and improved return on investment. The increased electrical efficiency – up to 45% Natural Gas (NG) / 43.6% Bio Gas (BG) makes the generator set more economical for customers as it burns less gas to produce even more energy.

“At Caterpillar, we have a laser sharp focus on customer success,” said Mark Jenzer, product manager with Caterpillar Energy Solutions. “We’re dedicated to research and development, constantly looking to see how we can re-engineer our products to help them better serve our customers. We are thrilled to announce the B series of CG170 gas generator sets, as they will do just that – help our customers achieve more and be more profitable.” 

“The B series offers high power density enabled through a compact design delivering greater return on investment,” said Jenzer. Advanced engineering improvements with the B series of the CG170 generator series includes switching from aluminum to steel pistons allowing for higher efficiency. Additionally, the air filters have been redesigned which supports the compactness of the generator set. “With upgraded state of the art technology, the B series of CG170 can provide up to 80,000 hours until major overhaul. This results in higher reliability and lower total owning and operating cost for customers," said Jenzer.

The CG170B series offers different engine variants tailor-made for a variety of applications - running on natural gas, biogas, wellhead and propane gas. “This offers greater flexibility to our customers allowing them to choose the type of fuel they want to use,” said Jenzer. “With the different engine variants, we can offer high-efficiency engines optimized for electrical efficiency at the lowest possible operating costs. We also offer a high response version which is optimized for total efficiency if a customer is interested in producing electrical energy, but also needs heat for internal efficiency by utilizing Combined Heat and Power (CHP).  The series also offers a biogas version where the engine has been optimized for total efficiency with a variety of biogases,” said Jenzer. In the future the CG170B will offer a variant for high altitude and ambient temperatures for regions of the world where climates are rough, we have optimized the engine to run in the harshest climates. 

The CG170B series features Caterpillar’s fully digitized Total Plant and Energy Management (TPEM) system. Responsible for controlling all power plant data within an advanced hardware and software solution, this new system eliminates the need for multiple controls. It also features a user-friendly 15-inch touchscreen, which provides a wide range of data concerning the status of the power plant. The data is saved for up to one year, enabling shorter maintenance times through systematic planning. 

The CG170B also comes standard with Cat® Connect capabilities, Cat Connect is a suite of services to collect and analyze data to help customers reduce owning and operating cost and increase profits.

Caterpillar Energy Solutions is announcing availability for the 20-cylinder version today, with 12 and 16 cylinders coming out later in 2019. Caterpillar is best in class in the power generation marketplace with market leading power systems engineered to deliver unmatched flexibility, expandability, reliability and cost-effectiveness. With parts and service available globally, Caterpillar offers worldwide product support through its comprehensive service and dealer network, where technicians are trained to service every aspect of the equipment.    

For more information, visit https://www.cat.com/catcg170b

 

# # #

 

About Caterpillar Energy Solutions

With its two brands, MWM and Cat, Caterpillar Energy Solutions stands for highly-efficient and eco-friendly solutions for distributed power generation and manufactures gas engines, electricity power plants, as well as CHP plants. As part of the Caterpillar Global Power Solutions Division, Caterpillar Energy Solutions today commands a leading market position in the field of highly efficient, ecologically advanced distributed energy solutions. Thus, we serve our customers around the globe as a reliable partner for proven and sustained added value in the implementation of power plant projects. Our products are the result of more than 145 years of experience in the development and optimization of gas engines and generator sets for natural gas, biogas and other special gases.

About Caterpillar

For more than 90 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent. Customers turn to Caterpillar to help them develop infrastructure, energy and natural resource assets. With 2017 sales and revenues of $45.462 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. The company principally operates through its three primary segments - Construction Industries, Resource Industries and Energy & Transportation - and also provides financing and related services through its Financial Products segment. For more information, visit caterpillar.com. To connect with us on social media, visit caterpillar.com/social-media.

Caterpillar. All Rights Reserved. CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Yellow”, the “Power Edge” and Cat “Modern Hex” trade dress as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

©2019 Caterpillar
All Rights Reserved

 

Press Inquiries

Sarah Pullen
Caterpillar Inc.
Tel: +1 309-675-1513
Pullen_Sarah_C@cat.com
Reader Responses

Caterpillar Inc.
Electric Power Division
P.O. Box 0610
Mossville, IL 61552-0610