Cat® dragline bucket
Cat® dragline bucket

Cat® Pin Grabber Couplers Boost Productivity, Reliability, and Keep Safety a Priority

 

 

For Release in North America, South America: April 2020
Release Number: 304PR20

Cat® pin grabber couplers bring a new level of productivity allowing the operator to change tools in a matter of seconds rather than minutes. Excavators of similar sizes can share attachments. With the addition of the VB and HB sizes of pin grabber couplers, there is now a coupler for every size of excavator from the 311 – 390. VB and HB refer to linkage sizes. Caterpillar classifies excavator fronts according to the “linkage family,” which is the size at the end of the stick. Pin grabber couplers are weighted to handle big payloads when added to a machine and bucket combination, without having to compromise on the bucket size.

Pin grabber couplers feature a redundant locking system, ensuring attachments are secure to the coupler. The spring-loaded arms keep the latch closed, even in the event of a hydraulic pressure loss. The shorter profile of the coupler helps keep the distance from the end of the machine’s stick to the tip of the bucket’s teeth compact, to maximize the amount of digging power you have with the addition of the coupler. The coupler frame’s cast pieces are made from abrasion-resistant steel to maintain the coupler’s durability over time.

The coupler has visual and audible cues for the operator to indicate it is secure to the attachment. The primary greasing block is the central greasing point for the whole coupler and is easily accessible at ground level. Operating procedures for the pin grabbers are intuitive and simple to learn for operators of all experience levels. Adding the versatility of a pin grabber coupler allows you to switch from digging, grading, material handling, compacting soil, breaking rocks, and more with ease. Using the pin grabber coupler also gives you the ability to pick a bucket up in reverse position to clean out square corners. 

 

Pin Grabber Coupler Specifications

 

Linkage/
Model Name

Minimum Carrier Weight

Maximum Carrier Weight

Coupler Weight

Tons

Tons

kg

lb.

312

11

15

188

414

315

15

18

299

659

B

19

23

380

837

CB-Trenching

24

35

430

949

CB

24

35

465

1025

DB-Narrow Profile

30

40

624

1376

DB

30

40

621

1370

TB-Trenching

45

52

934

2060

TB

45

52

944

2082

VB2

74

74

1244

2744

HB2

90

95

1556

3430

 

For a complete list of Pin Grabber Coupler models and specifications, visit cat.com.

 

of

VB-Linkage Pin Grabber Coupler

of

HB-Linkage Pin Grabber Coupler

of

Pin Grabber Coupler locking mechanism engaged

Product & Service News

See the latest product and engine announcements from Caterpillar.

See the Latest News

 

 

# # #

 

Note to Editors: Caterpillar rolls out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.

CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

©2020 Caterpillar All Rights Reserved

 

Press Inquiries

Caterpillar Trade Press Media Representatives

Americas

Sharon Holling: Holling_Sharon_L@cat.com

Johanna Kelly: Kelly_Johanna_L@cat.com

Europe, Africa, Middle East

Francine Shore: Shore_Francine_M@cat.com

Reader Requests
www.cat.com/requestCatinfo