Wet disk snubber upgrade cuts maintenance on Cat® rope shovels

Wet disk snubber upgrade cuts maintenance on Cat® rope shovels

For Release Worldwide: April 2019 
Release Number: 165PR19

Caterpillar recently introduced a new wet disk snubber upgrade for dipper doors on its 7495 Series electric rope shovels. The oil-filled snubber is maintenance and adjustment free for its 12,000-hour life before rebuild, which aligns with dipper service life.

The new snubber design—a sealed, oil-immersed clutch pack—eliminates a daily maintenance touchpoint and delivers much longer life than the standard snubber. Additionally, the wet disk snubber can be rebuilt three times before replacement is needed, and rebuilds are simpler and faster than standard snubber rebuilds.

The snubber plays a critical role in truck loading as it provides controlled resistance to the motion of the dipper door. During opening, the damping torque slows door velocity to prevent collisions with the truck body. During closing, the damping torque prevents the door from slamming against the dipper body and dipper structure.

The wet disk snubber results in reduced maintenance time and costs, improved reliability, enhanced safety, and lower total cost of ownership. In field validation at a Wyoming coal mine, wet disk snubbers also reduced frequency of repairs to the dipper door and latch keeper.

The wet disk snubber is retrofittable and available for both latched and LatchFree™ Cat® Dippers installed on Cat 7495, 7495 HF and 7495 HD Electric Rope Shovels. The snubber upgrade can be retrofit in about two days and is typically completed when the dipper is being rebuilt.

For more information, contact the local Cat dealer or your Caterpillar representative.

 

CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

VisionLink is a trademark of Trimble Navigation Limited, registered in the United States and in other countries.

©2019 Caterpillar. All Rights Reserved.

Press Inquiries

Caterpillar Trade Press Media Representatives

Americas

Sharon Holling: Holling_Sharon_L@cat.com

Johanna Kelly: Kelly_Johanna_L@cat.com

Europe, Africa, Middle East

Francine Shore: Shore_Francine_M@cat.com

Reader Requests

www.cat.com/requestCatinfo