Caterpillar Unveils the M 32 E, Increased Power Rating

For Worldwide Release: June 2013

 Release Number: M5PR13

Hamburg, Germany – Caterpillar Marine Power Systems is pleased to announce the development of the MaK™ M 32 E, a new high performance marine diesel engine platform for the commercial marine industry based on the highly successful M 32 C engine series. The M 32 E engine boasts an increased power rating of 550 kW per cylinder @ 720 and 750 rpm and with total output ranging from 3,300 kW for the six cylinder configuration to 4,950 kW for the nine cylinder configuration. First engine deliveries are foreseen for fall 2014.

“We’re pleased to offer our customers a more powerful yet still proven MaK engine solution,” said Carsten Seeburg, MaK product definition manager. “We were able to transfer many of the notable product attributes of the M 32 C, such as durability and simplicity, to the new platform and provide customers with an additional solution for their commercial applications.”

Offering both 720 & 750 rpm and the higher power output ideal for the offshore market in diesel electric and auxiliary applications with multi-engine concepts, the M 32 E is the first MaK “5 Mega Watt” power solution in the 320 mm bore segment. Additionally, the M 32 E is an ideal platform to drive variable speed diesel-electric systems and can be perfectly integrated with the proven Cat high speed engines in mixed engine rooms.

The engine features a stroke of 460 mm and utilizes the piston and other proven components from the VM 32 C and the same footprint as the M 32 C. In addition to having Heavy Fuel Oil (HFO) capability, the new M 32 E features the same lube oil consumption and maintenance intervals as the M 32 C product series. The engine is EPA Tier 2 and IMO II compliant.

The M 32 E with its high power output will fit perfectly in the comprehensive Cat product line between the efficient M 32 C and the fuel flexible M 34 DF. Caterpillar will offer its renowned service and support for the new MaK engine, including installation and application, system integration support, as well as customer and crew training. The M 32 E will pass customer acceptance tests and classification approvals in Kiel,  Germany and will be sold through Caterpillar’s MaK dealer network.

For more information about Caterpillar and MaK marine engines, please visit MARINE.CAT.COM/pr

# # #

About Caterpillar Marine Power Systems

Caterpillar Marine Power Systems, with headquarters in Hamburg, Germany, groups all the marketing and service activities for Cat® and MaK marine engines within Caterpillar Inc. The organisation provides premier power solutions in the medium- and high-speed segments with outputs from 93 to 16,800 kW in main propulsion and 10 to 16,100  kWe in marine generator sets. The sales and service network includes more than 2,100 dealer locations world-wide dedicated to support customers in ocean-going, commercial marine and pleasure craft wherever they are.

More information is available at: MARINE.CAT.COM/pr

Note to Editors: Caterpillar rolls-out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.

Press Inquiries

Caterpillar Marine Power Systems Communications
Jenna Janik: Janik_Jenna_E@cat.com

Reader Requests
www.cat.com/requestCatinfo