For Release in North America and Europe: January 2014
Release Number: 530PR13
The new Cat® M Series 3 motor graders—12M3, 140M3, 160M3 and their all-wheel-drive (AWD) counterparts—bring the latest emissions reduction technology to the most durable, productive and comfortable graders on the market. The new models offer greater fuel efficiency, more operator comfort and safety features, as well as enhanced serviceability. M Series 3 motor graders meet U.S. EPA Tier 4 Final/EU Stage IV emission standards.
Fuel Efficiency and Emissions Reduction
M Series 3 motor graders meet U.S. EPA Tier 4 Final/EU Stage IV emission standards using emissions reduction technology that is designed to be transparent, with no action required by the operator. There is no need to stop for regeneration. The system uses Caterpillar’s proven aftertreatment solution with the addition of Selective Catalytic Reduction (SCR). SCR utilizes Diesel Exhaust Fluid (DEF), which can be conveniently filled from ground level when the machine is fueled. Because of improved fuel economy over Tier 4 Interim and efficient use of DEF, M Series 3 motor graders deliver excellent overall fluid efficiency.
A new standard Economy (ECO) Mode can be turned on to help save fuel by reducing engine speed so the machine works in a more efficient range. The average fuel savings is up to 10 percent, depending on the application.
Integrated Technologies
Cat Connect makes smart use of technology and services to help improve jobsite efficiency. M Series 3 motor graders are equipped with Product Link™, which helps fleet owners track location, hours, fuel usage, productivity, idle time, and diagnostic codes through the online VisionLink® interface. M Series 3 machines also offer optional grade technologies like Cat Grade Control Cross Slope and Cat AccuGrade™ help operators work more efficiently, productively and accurately.
Comfort and Convenience
In the cab, operators will find the hallmark Cat motor grader controls—two electronic joysticks that reduce arm movement by 78% to help lessen operator fatigue and enhance productivity. M Series 3 models also feature a redesigned message display located in the center console of the machine. The display puts Cat Grade Control Cross Slope information conveniently in front of the operator, and also includes a DEF tank level gauge. Operators will also enjoy a more comfortable seat with heated and ventilated options, an optional seat belt indicator light, and several convenient new storage bins located throughout the cab. An additional convenience feature can be found in the engine compartment. New optional LED lights make it easier to service the machine in low light conditions.
For more information about Cat M Series 3 Motor Graders, contact the local Cat dealer or go to: http://www.cat.com/en_US/products/new/equipment/motor-graders.html.
M Series 3 Motor Grader Specifications
|
12M3/12M3 AWD |
140M3/140M3 AWD |
160M3/160M3 AWD
|