1of

Test

Test

Test Label

Test 1

Test 1

Test Desc 1

Test Label 1

Jobsite connectivity
Jobsite connectivity

Jobsite Connectivity – Is It Worth It?

 

 

“Today’s projects are ever more complex and larger in scale. Our analysis shows that large projects across asset classes typically take 20 percent longer to finish than scheduled and are up to 80 percent over budget. There are deep issues that can only be overcome with new ways of thinking and working.”

-Mukund Sridhar, partner, McKinsey & Company, 2016 Construction Technology Summit

 

Sridhar, as well as other industry analysts, cites studies reported by the Boston Consulting Group that show digital technologies have reduced cost and schedule overruns by 10 to 15 percent or more, as the level of project complexity rises. Where do these efficiency gains come from? Here’s a quick list of some of the most often identified technology-driven efficiencies.

 

 

Improved Equipment Utilization

When you can collect accurate data from your fleet, you can run utilization reports by asset type. Let's assume the fleet has 15 excavators. The data shows that:

- 8 of them are running at 80 percent utilization
- 4 of them are running at 50 percent utilization 
- 3 of them are running at 20 percent 

When your equipment is spread over a wide area or multiple locations, it's a bigger challenge to get an accurate read on how they're being used. But when that information is wirelessly communicated to you via the internet, you can see the numbers in black and white, in real time. 

In this case, it's easy to see that the operation doesn't need to add excavators. If excavator utilization was better managed, the operation may be able to park an excavator or two and free up the capital invested in excavators that weren't fully utilized, resulting in better cash flow and reduced cost of capital.

Equipment
Equipment
Reduced Fuel and Maintenance Costs

Service hours are one of the most monitored performance metrics. The problem with an hour reading is that it doesn't differentiate between "on time,"working time" and "idling time." When you can gather the telematics data from a connected machine, you have the opportunity to work with your operators to reduce idle time. Idle time reduction will dramatically cut your fuel bill in the short term and also give you a realistic usage barometer for that machine. Then you can begin to manage that machine based on the true hours worked, not just the hours on the meter. The result is a reduction in the number of maintenance cycles (Pms) required, which reduces cost.

Technician on Computer
Technician on Computer
Reduced Repair and Maintenance Costs

When you have the ability to access fault codes remotely, you and your techs can perform preliminary diagnoses without having to travel any futher than your smartphone or computer. After a thorough review of the data, you can decide the right course of action – once. You can communicate with the operator. Techs can gather the right tools and parts that will be needed before heading to the site. Your operation saves significantly in technician time and machine downtime.

Operator on Phone
Operator on Phone
What about GPS – Is it worth it?

Based on this quick list, it would seem that connectivity delivers sufficient cost savings to pay for itself. Let's extend the conversation beyond leveraging information to adding GPS earthmoving technologies to the mix. Is GPS worth it?

A Civil Engineering study found that GPS-enabled earthmoving can increase productivity by 21.74 percent and generate cost savings of approximately 12.92 percent. What does that translate into on the bottom line? If the cost of GPS set up on a dozer is approximately $100,000 on a $500,000 job, you'd save more than $60,000 – more than half of the cost of the system. Add to that more competitive bidding (results from accurate data) and faster job completion (resulting from efficiency gains), and breakeven should easily come within the first year of ownership.

Even with all these economic benefits, construction remains one of the least digitized of all industries. So, there's a real opportunity to build competitive advantage with connectivity on your jobsites – seems like it would be well worth the investment. 

Operator working with Technology
Operator working with Technology


Find our how you can make more money with Cat® Technology and Services from your Cat dealer.
 

Improve with Cat® Productivity

Cat Productivity gathers and analyzes Cat Production Measurement, machine and jobsite data from your equipment. Get more insight into your operations than ever before.

Get Connected
Cat Technology
Cat Technology
STAY INFORMED WITH CAT EQUIPMENT MANAGEMENT

Cat Equipment Management gives you access to a range of digital platforms that work in combination or independently — so you can stay informed and productive.

Learn More
Operator Training
Operator Training

RELATED ARTICLES

You’re here to get ideas to grow your business. Read on for machine insights and expert tips and tricks to get more out of every job.

warning

Internet Explorer users may experience issues with certain features of our site.
Please try a current version of an alternate browser (i.e. Google Chrome, Microsoft Edge, Mozilla Firefox) for the full Cat.com experience.