1of

Test

Test

Test Label

Test 1

Test 1

Test Desc 1

Test Label 1

Disaster brings innovative fuel solutions

linden
linden

Superstorm experience prompts bi-fuel option

Customer: City of Linden, New Jersey

Location: Linden, New Jersey, USA

Customer Business Issue: Standby power for outages as well as flexibility for peak shaving

Solution: Cat® C27 diesel generator set using dual-fuel technology

Cat® Dealer: Foley Power Systems

of

Cat® C27 generator set

of

“We felt that it would be economically advantageous to have a bi-fuel generator with the demand response capability.” Al Macdonald, director of Linden Public Property and Community Services

of

Cat® C27 bi-fuel generator installation

of

Foley Power has been on top of the entire project

POWER NEED

Years after Superstorm Sandy devastated the East Coast of the U.S. in the fall of 2012, many cities and towns are still dealing with the fallout. For the City of Linden, New Jersey– a municipality about 20 miles southwest of Manhattan with a population of more than 40,000—the storm underlined the need for a new source of emergency power.

“Immediately after Sandy hit, we were down for the better part of two weeks,” said Al MacDonald, director of public property and community services for the City of Linden. “We were 100 percent without grid power.”

Linden’s city hall building houses numerous important municipal functions, including the 911 dispatch center and most of the servers for the city’s computer system.

The city hall relied on a generator set from the 1970s to maintain power in the weeks following the storm. It soon became clear that the power need was too much for the aging generator set, requiring the use of several smaller rental generator sets to help support the load.

“It was obvious that city hall had a generator issue because of its age and what it lacked in power,” MacDonald noted. “We’ve had interruptions in the past, and fortunately we were pretty lucky with that old generator. We didn’t lose the critical systems like 911 dispatch and our computer system, but everything else pretty much came to a standstill at city hall.”

SOLUTION

Realizing an upgrade was long overdue, city officials worked with Cat dealer Foley Power Systems in 2016 to install a Cat C27 diesel generator set equipped with dual-fuel technology to help provide the robust backup and emergency power the building needed.

Generator sets that use dual-fuel technology extend run times and mitigate refueling issues by operating on a mixture of diesel and natural gas. In fact, a large percentage of the diesel fuel can be substituted with pipeline natural gas, providing at least twice the amount of run time from a stored volume of diesel fuel.

This allows users to reduce the amount of fuel stored on-site.

“We felt that it would be economically advantageous to have a generator using dualfuel technology with the capability to provide power during emergency utility outages, as well as for non-emergency purposes,” MacDonald said. “Our environmental consultant, Greener By Design, advised us that a dual-fuel generator with emissions controls would provide flexibility to participate in nonemergency energy market applications such as demand response, as well as mitigate risks related to diesel fuel delivery that had been an issue in the past.”

Because Linden intends to use the generator set in emergency and non-emergency modes, the municipality also needed to install emissions exhaust reduction equipment to comply with environmental regulations. The team mounted a selective catalytic reduction (SCR) aftertreatment system on the roof of the generator set’s outdoor enclosure to meet these requirements.

To help mitigate noise from the generator set both inside city hall and in the nearby residential neighborhood, it was surrounded by a sound-attenuated enclosure built to exceed local noise ordinances.

City officials also took advantage of two programs to help reduce the costs of installing and maintaining the new generator set. First, they reduced bidding time by using a cooperative purchasing program available through the National Joint Powers Alliance (NJPA), which is now known as Sourcewell. This member-owned cooperative establishes and provides nationally leveraged and competitively solicited purchasing contracts from industry-leading vendors to help government, education, and non-profit organizations save time and money on the negotiation process.

“The bidding is already done for you, so you know that you’re getting the best price for the piece of equipment that you spec out,” MacDonald said. “So not only did we get the best price, we got exactly what we specified.”

Second, the city signed a Customer Support Agreement (CSA) with Foley Power Systems for ongoing maintenance and service on the generator set.

“For a piece of equipment this critical to the continued operation of vital city systems and departments, it would have been foolish for us to not go with a maintenance agreement,” MacDonald explained. “Foley has been on top of the entire project from front to back. We’re more than pleased with how the whole project has been handled.”

RESULTS

“During events like Sandy when the city was down for 10 days, a dual-fuel system equipped with a multi-day tank of diesel fuel could have provided the city with full-time emergency power without having to fill the diesel fuel more than once,” said Scott Yappen, director of business development with Foley Power Systems. “So this dual-fuel solution should keep the City of Linden run ready for decades to come.”

Using the generator set for other nonemergency applications like demand response will also help relieve stress on the utility grid during times of peak consumption, such as hot summer days. When a demand reduction request is signaled, city officials can adjust power demand by postponing some tasks with large power demands or use the new generator set for peak shaving.

“Our research showed other facilities that have done a similar setup have offset their costs tremendously over a long period of time,” MacDonald said. “By participating in the energy market programs during times of peak usage, we anticipate recovering our cost over the long term.”

Download the Power Profile

Featured products

  • Maximum Rating
    800 ekW
    800 ekW
    Minimum Rating
    635 ekW
    635 ekW
    Emissions/Fuel Strategy
    Low Fuel, Tier 2 Nonroad Equivalent
    Low Fuel, Tier 2 Nonroad Equivalent

    C27 (60 Hz)

    The C27 diesel generator sets have been developed for your mission critical, standby and prime applications. Producing reliable power from 635 to 800 ekW at 60 Hz, each generator set has been designed to meet ISO 8528-5 transient response requirements and to take on 100 % block load. The C27 is certified as a low fuel consumption system as well as having a certificate for EPA Stationary Emergency (Tier 2).

    Learn More

Electric Power products

Any size or shape. In any regulatory environment. When you need power, Caterpillar is equal to the challenge. Our generators are used in a variety of applications.

View Electric Power products
electric power
electric power

Generator Set Sizing Calculator

Caterpillar Electric Power is excited to introduce you to our latest generator set sizing software, Cat Electric Power SpecSizer.

Learn More
specsizer
specsizer

Municipality

You’re trusted to provide the power your community lives on — and makes a living with. Whether it’s standby power for emergency use or additional systems to handle peak hours, be there when the people you serve need it most.

View Municipality Page
Municipality
Municipality

CAT DEALERS MAKE THE DIFFERENCE

Your Cat dealer is committed to maximizing your success, helping you get the most out of your operations with site-level solutions, service and support.

CONNECT WITH YOUR DEALER TODAY
dealers
dealers
warning

Internet Explorer users may experience issues with certain features of our site.
Please try a current version of an alternate browser (i.e. Google Chrome, Microsoft Edge, Mozilla Firefox) for the full Cat.com experience.