1of

Test

Test

Test Label

Test 1

Test 1

Test Desc 1

Test Label 1

From Trash to Treasure

cedar
cedar

Cat Generator Set Converts Landfill Waste into Energy

Customer: Cedar Rapids Linn County Solid Waste Agency

Location: Marion, Iowa

Customer Business Issue: U.S. Environmental Protection Agency (EPA) emission standards for landfills

Solution: Cat® G3520C gas generator set

Cat® Dealer: Altorfer

of

Cedar Rapids Linn County Solid Waste Agency

of

The 2242 horsepower Cat G3520C advanced gaseous-fueled generator set features high efficiency and long service life to support low-energy fuel from landfill applications.

of

Cat® G3520C gas generator set

of

A heat exchanger unit rests on a skid adjacent to the Cat generator enclosure.

POWER NEED

The Cedar Rapids Linn County Solid Waste Agency operates the 75-acre landfill in Marion, which serves 17 communities in the county. The facility includes a 44,000-square-foot resource recovery building that is used for processing hazardous household materials and transferring recycled materials.

When it started accepting waste from the entire county, the landfill near Marion developed quickly, with four new cells added between 2007 and 2013. The landfill currently accepts about 180,000 tons of municipal waste annually. In 2009, the agency installed a system of wells to collect methane gas from the original 30-acre cell and a 13-acre plot.

Landfill gas is typically made up of 50% methane, 50% carbon dioxide, and trace amounts of various hazardous air pollutants known as non-methane organic compounds (NMOCs). The EPA requires large landfills that emit NMOCs from landfill gas in excess of 50 megagrams (Mg) per year to control emissions.

SOLUTION

In general, controlling emissions involves drilling collection wells into the landfill and routing the gas to a suitable energy recovery system or combustion device. Combusting the landfill gas destroys most of the NMOCs in the gas while oxidizing the methane gas to carbon dioxide. This process also reduces the landfill’s greenhouse gas footprint since methane has a 25 times greater global warming potential compared to carbon dioxide.

Five years ago, Cedar Rapids Linn County Solid Waste opted to install a Cat G3520C gas generator set, which uses the methane as fuel to run the engine and rotate the generator, which produces electricity.

About 500,000 cubic feet of gas is consumed daily by the agency’s Cat generator set. Condensation is removed from the landfill gas before it is combusted in the engine. Otherwise, the gas receives essentially no pretreatment. One of the strengths of the Cat G3520C is the ability to run on relatively low concentrations of methane. The concentration of methane at the Marion landfill averages about 50 percent.

“This Cat engine is a lean burning unit, which means it has additional inerts within the gas stream,” says Garrett Prestegard, an environmental engineer with the Cedar Rapids Linn County Solid Waste Agency. “The inerts in the gas stream absorb heat during the combustion process, which reduces exhaust temperatures. This limits the formation of NOx emissions and helps us meet our air quality requirements. 

The 2242 horsepower Cat G3520C advanced gaseous-fueled generator set features high efficiency and long service life to support low-energy fuel from landfill applications. The G3520C 60 Hz generator set is specifically designed to protect engine components against landfill gas contaminants, eliminating the need for elaborate fuel-treatment systems and special maintenance and service practices. The G3520C generator set also provides a lower installed cost per kW, with power densities as high as 100 kW per cylinder.

RESULTS

The electric power produced by the Cat generator set is sold back to the local utility, Central Iowa Power Cooperative (CIPCO). Annual revenue generated from power production is more than $500,000.

“Having a gas system in place that diverts landfill gas to a control device which burns it off is greatly beneficial to the environment and public health because it reduces our emissions footprint,” says Prestegard. “To be able to collect landfill gas and not only burn it to help control our emissions, but have the added benefit of generating electricity and selling it to the grid is a very positive thing.”

By purchasing renewable energy, CIPCO enables its member systems like East Central Iowa REC to offer energy options. Nearly 60 percent of CIPCO’s electricity is generated from emission- and carbon-free resources, minimizing impact to the environment. All or some of the renewable energy credits associated with this generation may have been sold or will be sold in the future, to other parties, or may be used to comply with future regulatory requirements.

Waste heat generated from the power plant can be used directly by adjacent businesses. The Cedar Rapids Linn County Solid Waste Agency collects the excess heat from the Cat generator set to provide heating needs to its nearby 44,000-square-foot resource recovery building.

A heat exchanger unit rests on a skid adjacent to the Cat generator enclosure. There are two parallel coolant systems, one that runs through the engine and another one that runs through the heat exchanger to the resource recovery building. The heat is transferred from one coolant system to the other, and the heated coolant is piped back to the resource recovery building. At that point, it’s sent through a radiant heating floor system in the drivethrough aisle and is also sent to a snow-melt system adjacent to the truck bays outside. The generator waste heat is also used to provide heating through three makeup air units.

“Capturing the thermal energy and using it to heat our resource recovery building is a nice added benefit,” Prestegard says.

Cat dealer Altorfer provides all maintenance to the generator set through a 10-year Customer Support Agreement. That includes regularly scheduled maintenance, oil changes, spark plugs, top end in-frame overhauls, and a major overhaul, once the genset reaches 60,000 hours.

“We’ll be at the point where we have enough waste depth to go out and drill wells into those areas,” Prestegard says. “And when we do that, we certainly anticipate maxing out the capacity of our current engine. We’ll probably be at a stage where we will be collecting enough methane to support the installation of another Cat generator set.”

Download the Power Profile

Featured products

  • Continuous Rating
    1972 ekW
    1972 ekW
    Fuel Type
    Low Energy, Biogas, Coal Gas
    Low Energy, Biogas, Coal Gas
    Maximum Electrical Efficiency
    40.10%
    40.10%

    G3520C

    From low energy gas-fueled combined heat and power (CHP) systems and emergency power for facilities, to renewable biogas energy to support the local grid, or electricity generated from coal mine gases, Caterpillar has a wide range of reliable gas power solutions.

    Learn More

Electric Power products

Any size or shape. In any regulatory environment. When you need power, Caterpillar is equal to the challenge. Our generators are used in a variety of applications.

View Electric Power products
electric power
electric power

Generator Set Sizing Calculator

Caterpillar Electric Power is excited to introduce you to our latest generator set sizing software, Cat Electric Power SpecSizer.

Learn More
specsizer
specsizer

Landfills

Power your world with sustainable practices. Cat generator sets are designed to collect, clean and run on harmful gases produced by landfills. It’s reliable power that promises to reduce your environmental impact.

View Landfills Page
Landfills
Landfills

CAT DEALERS MAKE THE DIFFERENCE

Your Cat dealer is committed to maximizing your success, helping you get the most out of your operations with site-level solutions, service and support.

CONNECT WITH YOUR DEALER TODAY
dealers
dealers
warning

Internet Explorer users may experience issues with certain features of our site.
Please try a current version of an alternate browser (i.e. Google Chrome, Microsoft Edge, Mozilla Firefox) for the full Cat.com experience.