Landfill Gas to Energy

hangzhou
hangzhou

Landfill Gas as a Renewable Fuel Source

 

Client: Hangzhou Municipal Solid Waste Treatment Company Ltd.

Location: Hangzhou, Zhejiang, China

Solution: Cat® G3516

Cat Dealer: Lei Shing Hong Machinery

 

of

Hangzhou Municipal Solid Waste Treatment Company Ltd.

of

The G3516 generator sets have demonstrated a reliability and availability that rivals even most natural gas engines.

Power Need

In the late 1990s, the Chinese government implemented reforms to help aide in the growth of the country's rapidly expanding economy. One of these reforms was an energy plan that would help ensure a more robust, consistent power grid. To achieve this, the government offers electricity production tax incentives. In addition to improving access to electricity, government officials wanted to increase the use of renewable fuel sources instead of continuing to rely on coal-fired power plants.

A ready source of renewable fuel is landfill methane, a byproduct of the decomposition of landfill waste. In recent decades, China has turned to using sanitary landfills, which are specifically designed to prevent contamination of groundwater and surrounding soil with a lining system. At these sites, waste is deposited in specific areas, and compacted and covered on a near-daily basis. The highly planned and managed nature of these landfills makes methane collection much easier than at old-fashioned dumping sites.

Solution

Hangzhou Municipal Solid Waste Treatment Company Ltd. operates multiple landfills in Hangzhou, China. In 1998, an outside waste-to-energy agency took advantage of the tax incentives and developed China's first landfill gas-to-power generation project at one of Hangzhou Municipal Solid Waste Treatment Company's landfill sites. The agency contracted with local Cat® dealer Lei Shing Hong Machinery to supply and install two Cat G3516 generator sets, each rated at 970 kW, and paralleling switchgear.

“These generator sets have been running successfully for more than 10 years and recently underwent their first major overhaul in 2011,” indicated Zoey Wang, Caterpillar Gas Territory Manager for China. “The G3516 generator sets have demonstrated a reliability and availability that rivals even most natural gas engines.”

Because of the success of this project, two more Cat G3516 generator sets, rated at 1030 kW, were installed at a second landfill site in 2009 and commissioned in March 2011. The installation is very similar to the first project. Based on estimates of landfill gas production, the customer expects to realize a future total production capacity of 8.4 MW.

Results

The two landfill power plants currently export approximately 4 MW of electricity back to the local grid, enough to power 20,000 average Chinese homes. Through Customer Support Agreements with the developers, Cat dealer Lei Shing Hong has kept the generators running smoothly, helping contribute to the increased reliability of the local power grid. Because this was the first landfill gas-to-power generation installation in the country, the support of Lei Shing Hong was instrumental in ensuring the project's success.

Download the Power Profile

Featured products

  • Maximum Rating
    660 BHP
    492 bkW
    Rated Speed
    1200 rpm
    1200 rpm
    Emissions
    Rich Burn: EPA NSPS Site Compliant Capable with Customer Supplied AFRC and Customer Supplied Aftertreatment or Standard Emissions for Export Only
    Rich Burn: EPA NSPS Site Compliant Capable with Customer Supplied AFRC and Customer Supplied Aftertreatment or Standard Emissions for Export Only

    G3516 NA

    The line of G3500 engines brings versatility, uptime, and low operating cost to your gas compression operation. They are equipped with ADEM A3 technology that enables highest performance and safety while maintaining low emissions. Ideal applications for G3500 engines include gas lift, gas gathering, and wellhead gas compression. Cat G3516 gas engine. Ratings: 492-1000 bkW (660-1340 bhp) @ 1200-1400 rpm are NSPS site compliant capable with customer-provided air-fuel ratio control and aftertreatment.

    Learn More
  • Maximum Rating
    1380 BHP
    1029 bkW
    Rated Speed
    1400 rpm
    1400 rpm
    Emissions
    Rich Burn: EPA NSPS Site Compliant Capable with Caterpillar Supplied AFRC and Customer Supplied Aftertreatment
    Rich Burn: EPA NSPS Site Compliant Capable with Caterpillar Supplied AFRC and Customer Supplied Aftertreatment

    G3516 TA

    G3516 TA Gas Engine

    Learn More

Electric Power products

Any size or shape. In any regulatory environment. When you need power, Caterpillar is equal to the challenge. Our generators are used in a variety of applications.

View Electric Power products
electric power
electric power

Generator Set Sizing Calculator

Caterpillar Electric Power is excited to introduce you to our latest generator set sizing software, Cat® Electric Power SpecSizer.

Learn More
specsizer
specsizer

Landfills

Power your world with sustainable practices. Cat® generator sets are designed to collect, clean and run on harmful gases produced by landfills. It’s reliable power that promises to reduce your environmental impact.

View Landfills Page
Landfills
Landfills

CAT® DEALERS MAKE THE DIFFERENCE

Your Cat dealer is committed to maximizing your success, helping you get the most out of your operations with site-level solutions, service and support.

CONNECT WITH YOUR DEALER TODAY
dealers
dealers
warning

Internet Explorer users may experience issues with certain features of our site.
Please try a current version of an alternate browser (i.e. Google Chrome, Microsoft Edge, Mozilla Firefox) for the full Cat.com experience.