1of

Test

Test

Test Label

Test 1

Test 1

Test Desc 1

Test Label 1

Power Repurposed

raleigh healthcare
raleigh healthcare

New Energy Plant and Generator Sets Power Raleigh Healthcare System

Customer: UNC REX Healthcare

Location: Raleigh, North Carolina, USA

Customer Business Issue: Expanded standby power capabilities to support growing medical campus

Solution:

Two Cat® C175-16 diesel generator sets

One Cat 3516 generator set

One Cat C175-20 generator set

Cat® Dealer: Gregory Poole Power Systems

of

NC healthcare system

of

Cat® generator sets offer reliable standby power for Raleigh, NC healthcare system.

of

Jeff Carter, director of facilities, construction, and biomedical engineering at UNC REX Healthcare.

of

The power plant can generate 12.25 MW of power.

of

The Cat® C175-20 diesel generator set is often used for large, mission-critical installations.

POWER NEED

Based in Raleigh, North Carolina, UNC REX Healthcare is a private, not-for-profit healthcare system that supports an acute care hospital, five wellness centers, two skilled nursing facilities and numerous other medical facilities throughout Wake County.

UNC REX Healthcare was the first hospital in the Triangle to be designated a Magnet hospital, which recognizes quality patient care, nursing excellence and innovations in professional nursing practice. In 2017, UNC REX Healthcare received a five-star rating from the Centers for Medicare & Medicaid Services, placing it among the top 9.1 percent of hospitals nationwide.

In the mid-2010s, UNC REX Healthcare officials planned a multi-year expansion at its medical campus in Raleigh – including the construction of the new eight-story, 306,000-square-foot North Carolina Heart & Vascular Hospital. To meet the growing power demand needed to support the highest level of care, leaders decided to build a new 17,000-square-foot energy plant that would repurpose standby power equipment already in use while adding new diesel generator sets offering industryleading power density.

SOLUTION

UNC REX Healthcare officials purchased two Cat C175-16 diesel generator sets for the power plant to join a Cat 3516 generator set that was relocated from the basement of the existing hospital. A Cat C175-20 generator set was added later to support the Heart & Vascular Hospital. The high power density of the 4 MW Cat C175-20 diesel generator set is a key benefit for standby power used in many large, mission-critical installations, such as data centers and hospitals.

“We have a long, ongoing partner relationship with our Cat dealer, Gregory Poole,” said Jeff Carter, director of facilities, construction and biomedical engineering at UNC REX Healthcare. “We’ve had a very good relationship with them for many years, and it was pretty much decided that we were going to use Cat generators at the beginning of this project.”

The power plant can generate 12.25 MW of power – more than enough to cover the entire electrical load of the campus.

“If we lose our main utility power source, these generators will automatically kick on within 10 seconds or less and provide full power to the hospital,” Carter noted.

RESULTS

As many as eight to 10 times a year when inclement weather threatens, the operations staff of UNC REX Healthcare follows storm running protocols by switching over to the facility’s own power sources.

“An office building or other businesses can ride through a storm having their power blink on and off a little bit, but we can’t because we’re a hospital,” said Michael Brailsford, manager of plant and energy operations for UNC REX Healthcare. “We have doctors who are operating and other procedures going on, such as people who are on life support, so we must maintain as smooth a flow of power as possible.”

Also, UNC REX Healthcare has an agreement with Duke Energy to generate 75 percent of its own load when called upon by the utility. These requests are typically made during periods of extreme ambient cold or heat when there is a higher demand for grid power.

The generator sets are tested weekly by the UNC REX Healthcare facilities staff to ensure they are in proper working order. Every other week, the staff performs a base load test where 30 percent of the capacity of each of the generator sets is utilized, running three at a time. On alternating weeks, they isolate the campus’ load from the grid and run the generator sets for an hour at full load.

While UNC REX Healthcare staff perform routine maintenance, all regularly scheduled maintenance is performed by Gregory Poole Power Systems as part of a Customer Support Agreement (CSA) with the hospital.

“We have operators who have basic knowledge of the maintenance that needs to be done on the generator sets, but Gregory Poole has highly skilled service technicians who can come in and work on these engines at any time. They pretty much know them inside and out,” Carter observed.

Download the Power Profile

Featured products

  • Standby Rating
    1750 ekW
    1750 ekW
    Prime Power Rating
    1600 ekW
    1600 ekW
    Emissions/Fuel Strategy
    Low Fuel, Low Emissions
    Low Fuel, Low Emissions

    3516 (60 Hz)

    Producing reliable power from 1450 to 1750 ekW at 60 Hz, our 3516 diesel generator sets are made to meet your mission critical, continuous, prime and standby applications. We've designed each to ISO 8528-5 transient response requirements and to accept 100% rated load in one step. Generator sets offer both low fuel consumption and low emission systems.

    Learn More
  • Standby Rating
    3365(no fan)/3250/3100(no fan)/3000 ekW
    3365(no fan)/3250/3100(no fan)/3000 ekW
    Prime Power Rating
    3115(no fan)/3000/2825(no fan)/2725 ekW
    3115(no fan)/3000/2825(no fan)/2725 ekW
    Emissions/Fuel Strategy
    Low Fuel, Tier 2
    Low Fuel, Tier 2

    C175-16 (60 Hz)

    Producing reliable power from 2500 - 3365 ekW at 60 Hz, our C175-16 diesel generator sets are made to meet your mission critical, continuous, standby and prime applications. We've designed each to ISO 8528-5 transient response requirements and to accept 100% rated load in one step. The generator set is Low Fuel Consumption, U.S. EPA Certified for Stationary Emergency Use Only (Tier 2 Nonroad Equivalent Emission Standards) certified.

    Learn More
  • Standby Rating
    4000 (no fan)/3900/3620(no fan)/3500 ekW
    4000 (no fan)/3900/3620(no fan)/3500 ekW
    Prime Power Rating
    3600 (no fan)/3500/3300 (no fan)/3180 ekW
    3600 (no fan)/3500/3300 (no fan)/3180 ekW
    Emissions/Fuel Strategy
    Low Fuel, Tier 2
    Low Fuel, Tier 2

    C175-20 (60 Hz)

    Producing reliable power from 3150 - 4000 ekW at 60 Hz, our C175-20 diesel generator sets are made to meet your mission critical, continuous, standby and prime applications. We've designed each to ISO 8528-5 transient response requirements and to accept 100% rated load in one step. The generator set is certified for low fuel consumption, U.S. EPA Stationary Emergency Use only.

    Learn More

Electric Power products

Any size or shape. In any regulatory environment. When you need power, Caterpillar is equal to the challenge. Our generators are used in a variety of applications.

View Electric Power products
electric power
electric power

Generator Set Sizing Calculators

Caterpillar Electric Power now has two tools available for sizing gensets in any application. 

Size Now
specsizer
specsizer

Healthcare

You power the machines that sustain lives. Install a generation system that not only promises continuous power but has the history to prove it. 

View Healthcare page
Healthcare
Healthcare

CAT® DEALERS MAKE THE DIFFERENCE

Your Cat dealer is committed to maximizing your success, helping you get the most out of your operations with site-level solutions, service and support.

CONNECT WITH YOUR DEALER TODAY
dealers
dealers
warning

Internet Explorer users may experience issues with certain features of our site.
Please try a current version of an alternate browser (i.e. Google Chrome, Microsoft Edge, Mozilla Firefox) for the full Cat.com experience.