If you already have an existing account with another Cat App, you can use the same account to sign in here.
One Account. All of Cat.
If you already have an existing account with another Cat App, you can use the same account to sign in here.
Account Information
Site Settings
Security Settings
TierPoint has one of the largest and most geographically diversified footprints in the nation. Its services include colocation, cloud computing, backup and business continuity, managed security, firewall, and professional services.
Learn MoreDoclerWeb turned to the local Cat® Dealer Huntraco for an integrated power system including a Cat 300 Series Uninterruptible Power Supply (UPS) unit and a Cat 3516B-HD 2500 kVA diesel generator set.
Learn MoreIn designing its data center, the company sought to create an environmentally friendly facility with a low- to zero-carbon footprint supported by cutting-edge green technologies. For example, instead of cooling the data center with traditional, energy-intensive air conditioning systems, the facility is cooled using evaporative cooling technology. This step alone results in a 50 percent electricity savings when compared to traditional data centers. As with any data center, Global Relay also needed a robust, reliable backup power system, but one that was as ecologically friendly as possible.
Learn MoreWhen Scott Data Center required a reliable standby electric power system for an additional 30,000-square-foot power plant, they worked with their local Cat® dealer to install 20 MW of cat power controlled by a customized switchgear system. “Since its installation in 2012, we have had zero problems—it has worked flawlessly.”
Learn MoreIntergate.Manhattan provides data management for its customers. It is supported by four Cat® C175 diesel generator sets that provide emergency power systems for critical operations. Equipped with a four-stroke-cycle diesel engine, the C175 is designed for reliable uptime and works with an integrated control system for improved performance.
Learn MoreThe Shanghai TCDC natural gas distributed generation project has Two Cat® G3520H gas engine gensets with a full load rating of 2,500, providing reliable power, efficiency, and low cost of operation and maintenance. The combined cooling, heating and power (CCHP) system simultaneously provides power and chilled water, meeting all power and cooling needs.
Learn MoreAs the nerve center for the company’s global operations, SAS headquarters in Cary, North Carolina, USA, requires reliable power for the computer, networking and phone systems essential to ongoing software development, technical support, sales and other business operations.
Learn MoreTo better support the IT department, CHI St. Alexius Health designed and built the Technology and Education Center, including a new server room, data center and standby power system, with energy efficiency in mind.
Learn MoreTo ensure its back-up power systems are reliable, and to meet on going service and support, i/o selected Caterpillar and Cat® Dealer Empire Power Systems to provide back-up power system solutions for its data centers in Phoenix and Scottsdale, Arizona.
Learn More