1of

Test

Test

Test Label

Test 1

Test 1

Test Desc 1

Test Label 1

Caterpillar Launches New Cat® XQ330 Mobile Generator Set Meeting Advanced Global Emissions Standards

For Release: February 2023

IRVING, TEXAS Caterpillar Inc. today announced the introduction of the Cat® XQ330 mobile diesel generator set, a new power solution for standby and prime power applications that meets U.S. EPA Tier 4 Final emission standards.

Powered by the efficient Cat C9.3B diesel engine, the XQ330 is rated for up to 288 kW in standby and 264 kW in prime operation at 60 Hz, and up to 341 kVA in standby and 310 kVA in prime power applications at 50 Hz.

Engineered to operate at lower noise levels than competitive offerings, the XQ330 packages essential components in a weather-resistant enclosure that streamlines transport, deployment, and maintenance while offering exceptional sound attenuation. It is also equipped with numerous rental-ready features, including a block heater, battery charger, permanent magnet generator (PMG), switchable voltage outputs, and optional mounting on a trailer.

The XQ330 is equipped with the EMCP 4.4 digital control panel, which provides all generator set controls and system indicators in a single, easy-to-access interface, as well as a programmable logic controller (PLC) functionality that improves reliability and flexibility for accommodating changes in processes or application requirements. Additionally, it includes fully featured power metering, protective relaying, engine, and generator parameter viewing.

It is equipped with Cat Connect technology to remotely track and manage the generator set and improve operational efficiency. The telematics send real-time information on fuel level, diesel exhaust fluid (DEF) level, battery voltage, and run status. Connected assets support peak operation with timely insights that help customers better control costs, improve performance, and reduce risks.

Cat diesel mobile generator sets meeting U.S. EPA Tier 4 Final standards can use up to 100% hydrotreated vegetable oil (HVO), a renewable diesel fuel meeting EN15940.

“Caterpillar has built a reputation for offering customers mobile power solutions with exceptional versatility, and the Cat XQ330 is equipped with a wide range of easy-to-operate features designed for numerous applications while meeting stringent emissions standards,” said Tom Caldwell, global general manager for electric power rental solutions at Caterpillar.

For more information about Caterpillar’s complete range of rental power solutions, visit www.cat.com/rentalpower or e-mail Electric_Power@cat.com.

of

Cat® XQ330 mobile generator set

Product and Services News

See the latest product and engine announcements from Caterpillar.

See the Latest News

 

###

 

About Caterpillar

With 2021 sales and revenues of $51.0 billion, Caterpillar Inc. is the world’s leading manufacturer of construction and mining equipment, off-highway diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. For nearly 100 years, we’ve been helping customers build a better, more sustainable world and are committed and contributing to a reduced-carbon future. Our innovative products and services, backed by our global dealer network, provide exceptional value that helps customers succeed. Caterpillar does business on every continent, principally operating through three primary segments – Construction Industries, Resource Industries and Energy & Transportation – and providing financing and related services through our Financial Products segment. Visit us at caterpillar.com or join the conversation on our social media channels.

© 2022 Caterpillar. All Rights Reserved. CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

Press Inquiries

Bob Chase
Gelia
Tel: +1 716-629-3230
bchase@gelia.com

Steve McDonagh
Caterpillar Inc.
steve.mcdonagh@cat.com

   

 

 

warning

Internet Explorer users may experience issues with certain features of our site.
Please try a current version of an alternate browser (i.e. Google Chrome, Microsoft Edge, Mozilla Firefox) for the full Cat.com experience.