Advanced Cat® Grade technologies expanded to Cat 6- to 10-ton next generation mini hydraulic excavators

 

For Release in North America, Europe, Australia and New Zealand: November 2021
Release Number: 845PR21

Caterpillar now offers Cat® Grade technologies as an aftermarket option to owners of Cat next generation mini hydraulic excavators in the 6- to 10-ton class range. Available through Cat and Sitech dealers, owners can equip the excavators with Cat Grade with Advanced 2D or Cat Grade with 3D. The field kit’s modular components facilitate quick installation, while the technology seamlessly integrates into the Cat next generation excavator electronics infrastructure.

Both aftermarket grade technologies mirror the capabilities of larger Cat excavators operating Cat Grade with Advanced 2D or 3D systems, allowing the equipment to reach target grade quickly. A separate, 254-mm (10-in) high-resolution touchscreen monitor allows operators to conveniently view, create and work site designs inside the cab. Automatics deliver simple, single-joystick control over the stick and bucket to maintain grade and avoid overcutting and undercutting.

Cat Grade with Advanced 2D uses on-board processors and fast-response sensors to deliver real-time bucket tip and elevation guidance on the touchscreen monitor. This technology gives operators the ability to create and work to basic site designs, while grade design edits can easily be made from the operator’s seat. Field installation of the technology includes the hardware, sensors and dedicated monitor for grade plan creation, editing and viewing.

Using GPS and GLONASS systems to pinpoint the excavator’s exact location, Cat Grade with 3D allows multiple machines to grade to complex jobsite designs. The monitor shows bucket position throughout the full range of the digging motion, while height and depth audio alerts indicate when desired grade has been reached to protect from overcutting or undercutting. Beyond the hardware and sensors, including monitor, required for Grade with Advanced 2D, installation of Grade with 3D also requires GNSS receivers and antennas.

Beneficial in a range of applications including sewer and septic work, digging footings and flat pad home development, Cat Grade technologies help operators reduce the number of passes and shortens the time it takes to complete cuts. They improve grade quality and consistency for operators of all experience levels and can extend the workday by aiding work in limited visibility situations. Saving costs associated with time, labor, fuel and material consumption, Cat Grade technologies allow companies to reach target grade quickly and lower overall operating costs at the jobsite.

More information on Cat Grade with Advanced 2D and Cat Grade with 3D for Cat 6- to 10-ton class mini hydraulic excavators can be found by contacting the local Cat-Sitech dealer or visiting: https://www.cat.com

 

Cat Grade for 6-9-ton Mini Excavators

 

 

Product & Service News

See the latest product and engine announcements from Caterpillar.

See the Latest News

 

# # #

Note to Editors: Caterpillar rolls out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.

CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

©2021 Caterpillar All Rights Reserved 

 

Press Inquiries

Caterpillar Trade Press Media Representatives

Americas

Sharon Holling: Holling_Sharon_L@cat.com

Johanna Kelly: Kelly_Johanna_L@cat.com

Europe, Africa, Middle East

Francine Shore: Shore_Francine_M@cat.com

Reader Requests

www.cat.com/requestCatinfo