Cat® 794 AC mining truck
Cat® 794 AC mining truck

Autonomous Cat® 794 AC mining truck equipped with Cat® MineStar™ Command for hauling makes its MINExpo debut

 

For Release Worldwide: September 2021
Release Number: 749PR21



Since the Cat® 794 AC electric drive truck debuted at MINExpo 2016, the global fleet has logged more than 780,000 hours of field operation, averaging physical availability of 90%. Offering up to 8% better payload and faster speed-on-grade, the 794 AC delivers up to 10% more productivity than competitive trucks. The 794 AC truck field fleet has tripled over the last two years to more than 150 units with the highest-hour truck logging more than 52,000 hours. They are working in coal and hard rock, deep pit and flat haul sites at low and high altitudes and operating in poor underfoot conditions in nine countries covering four continents.

In 2021, the Cat 794 AC returns to MINExpo, as the latest autonomous mining truck equipped with Cat® MineStar™ Command for hauling, an autonomous hauling solution. The 794 AC is the first electric drive model to join the expanding Command for autonomous haulage fleet, which includes the Cat 789D, 793D, 793F and 797F models.  

Autonomy is rapidly emerging in the mining industry as essential for improving safety and productivity and lowering cost. The 794 AC, equipped with Command for hauling, enables total autonomous operating of the mining trucks, interaction with other equipment, and integration with customer mining processes and systems, all managed by MineStar.

A Caterpillar designed technology, Command for hauling is a complete system integration offered from the factory. The software, systems, individual components and engine of the 794 AC are designed and supplied by Caterpillar and supported by the Cat dealer network. This integration ensures that the entire truck from body to bumper and engine to electronics can be fully optimized to deliver the lowest cost per ton.

Demonstrating up to a 30% productivity improvement over operator-driven models at mine sites around the world, Command addresses many mining challenges, including labor shortages and the demand for higher machine utilization. Autonomous trucks using Command for hauling recently surpassed 3-billion tonnes hauled with no lost-time injuries associated with automated truck operation, enhancing safety at the site. Command also supports the mine’s sustainability efforts through lessening infrastructure needs and reducing truck fuel burn, machine downtime and wear parts replacement.

First deployment to South America

The first autonomous 794 AC electric drive mining trucks are being deployed in South America. In Chile, the first of 28 autonomous 794 AC trucks began arriving in May 2021 to be part of Teck Resources Limited’s low-cost, long-life Quebrada Blanca Phase 2 (QB2) copper project. ­­

At the Quellaveco copper mine operated by Anglo American in the Moquequa Region of southern Peru, sixteen 794 AC trucks have been deployed and will reach a total of 27 trucks by 2022. As a new greenfield mine, they saw the value and flexibility in using the 794 AC in both modes of operation: operator-driven and fully autonomous. Pre-mining activities began earlier this year, with both operator-driven and autonomous trucks being utilized from the start.

  One of the largest undeveloped copper deposits in the world, Quellaveco has ore reserves of 1,3B tonnes (1.46B tons) at an average grade of 0.57% total copper. Copper reserves are 7,5M tonnes (8.4M tons), enough copper for 90 million electric vehicles. With first copper production scheduled for 2022, initial throughput capacities at Quellaveco are projected to produce 300 000 tonnes (336,000 tons) average of copper per year for the first 10 years of operation.

Quellaveco collaborated with Caterpillar and Cat dealer, Ferreyros, to find the most productive hauling solution at the mine for lowering total cost of ownership. Commenting on the project, David Rea, general manager, Cat large mining trucks, said, “The ongoing success at Quellaveco requires extensive subject matter expertise from a diverse team of Anglo American, Quellaveco, Caterpillar and Ferreyros personnel. The Quellaveco opportunity highlighted the importance of understanding the customer’s business needs and responding with a solution that meets their expectations.”

Non-autonomous trolley advantages

As a consideration for mines to further reduce energy consumption and reduce carbon emissions, Caterpillar offers the Cat Trolley Assist System for non-autonomous ultra-class electric drive mining trucks and will have more information on the system at MINExpo 2021. When connected to a trolley system, the truck’s propulsion system becomes powered purely with electricity from the power grid, using the full potential of the wheel motors and lowering fuel burn.

Compatible with operator-driven 794 AC mining trucks, the Cat trolley assist attachment is fully designed, integrated and built to Caterpillar specifications, so it leverages 100% of the AC drive train. The attachment includes a purpose-built trolley structure, pantographs, support systems and components to fully integrate the attachment to the 794 AC.

The trolley system reduces fuel burn by more than 90% while on trolley, lowering CO2 emissions by 20 to 60% and saving up to 40 l (10.5 gal) of diesel per cycle per 1 km (0.62 mi) of trolley line. At the same time, operating on the trolley line delivers faster cycle times and higher productivity with up to 100% speed-on-grade improvement compared to diesel mode.

More information about the Cat 794 AC electric drive mining truck, Command for hauling and Trolley Assist System can be found by talking to a Cat truck team member during MINExpo, contacting a regional Cat dealer or visiting: https://www.cat.com

 

of

The Cat 794 AC Mining Truck is equipped with Cat® MineStar™ Command for hauling, an autonomous hauling solution.

of

The Cat 794 AC Mining Truck is equipped with Cat® MineStar™ Command for hauling, an autonomous hauling solution.

of

The Cat 794 AC Mining Truck is equipped with Cat® MineStar™ Command for hauling, an autonomous hauling solution.

of

The Cat 794 AC Mining Truck is equipped with Cat® MineStar™ Command for hauling, an autonomous hauling solution.

of

The Cat 794 AC Mining Truck is equipped with Cat® MineStar™ Command for hauling, an autonomous hauling solution.

of

The Cat 794 AC Mining Truck is equipped with Cat® MineStar™ Command for hauling, an autonomous hauling solution.

 

 

 

 

Product & Service News

See the latest product and engine announcements from Caterpillar.

See the Latest News

 

# # #

 

CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

©2021 Caterpillar All Rights Reserved 

 

Press Inquiries

Caterpillar Trade Press Media Representatives

Americas

Sharon Holling: Holling_Sharon_L@cat.com

Johanna Kelly: Kelly_Johanna_L@cat.com

Europe, Africa, Middle East

Francine Shore: Shore_Francine_M@cat.com

Reader Requests

www.cat.com/requestCatinfo

 

 

 

warning

Internet Explorer users may experience issues with certain features of our site.
Please try a current version of an alternate browser (i.e. Google Chrome, Microsoft Edge, Mozilla Firefox) for the full Cat.com experience.