Cat® Command remote control operation
Cat® Command remote control operation

Cat® Command remote control operation expands to Cat 349, 352, 374 and 395 large excavators

 

For Release in Europe, Australia, and New Zealand: November 2022
Release Number: 772PR22

Cat® 349, 352, 374 and 395 large hydraulic excavators can now be equipped with Cat Command for Excavating. The remote-control system removes operators from potentially hazardous jobsite conditions by keeping them at a safe distance, and it reduces potential safety risks from climbing on and off machines.

The Cat Command station allows for non-line-of-sight remote control, where users can comfortably control all basic machine functions like digging, lifting and tracking. Additionally, Caterpillar exclusive machine technologies like Cat Grade with 3D for Excavators, Grade with Assist for boom and bucket, Swing Assist, E-Fence, and others can be set, activated, and used remotely.

The technology helps improve machine productivity on various projects like operating in unstable underfoot conditions, brownfields, shore work, and demolition. It also allows production to restart immediately following disruptive processes such as blasting in quarry applications.

Flexible, precise control

The Cat Command station provides non-line-of-site operation from the comfort of an air-conditioned office on site or many miles away. Distance is limited only by the capabilities of the network. The Cat Command station comfortably seats the operator in a customized “virtual cab” with familiar controls and machine displays. Users can control up to five different machines, one at a time, at the same or other locations, reducing downtime for shift changes or the need to travel to the jobsite. Touchscreen monitors similar to the in-cab displays offer the same machine information and access to machine setting just like in the machine. Screens mounted in front of the user provides an easy view of the excavator’s camera feeds.  

By removing the operator from the cab, Cat Command for Excavating offers a solution to workforce shortages and training advantages for newer operators. It opens opportunities to those with physical limitations that prevent them from climbing into the equipment, attracting a new generation of workers, and increasing the longevity of experienced operators.

The new large hydraulic excavator models join the existing Cat Command-ready excavators (320-340) and medium dozers (D5- D7) which can be operated from the same Command station.

More information about Cat Command for Excavating can be found by contacting a Cat dealer.

 

 

of

Cat® Command Stations being used to remotely control excavators at a river terminal to unload barges and ship cargo holds.

View Full Size Image
of

Cat® Command Stations in an office environment being used to remotely control excavators.

View Full Size Image
of

Cat® excavator working in the cargo hold of a ship by remote control.

View Full Size Image
of

Cat® excavator working at a building demolition project by remote control.

View Full Size Image

Product & Service News

See the latest product and engine announcements from Caterpillar.

See the Latest News

 

# # #

 

Note to Editors: Caterpillar rolls out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.

CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, VisionLink, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

©2022 Caterpillar All Rights Reserved 

 

 

Press Inquiries

Caterpillar Trade Press Media Representatives

Americas

Johanna Kelly: Kelly_Johanna_L@cat.com

Europe, Africa, Middle East

Francine Shore: Shore_Francine_M@cat.com

Reader Requests

www.cat.com/requestCatinfo

 

warning

Internet Explorer users may experience issues with certain features of our site.
Please try a current version of an alternate browser (i.e. Google Chrome, Microsoft Edge, Mozilla Firefox) for the full Cat.com experience.