Caterpillar autonomously hauls more than 1 billion tonnes of material with Cat® Command for hauling in less than a year

Trucks equipped with Command surpass the 4 billion tonne mark with no loss-time injuries 

 

For Worldwide Release: March 2022
Release Number: 95PR22

For the first time in mining history, trucks equipped with Cat® MineStar™ Command for hauling have autonomously moved more than 1 billion tonnes of material in less than a year. Roughly 1.2 billion tonnes (1.3 billion tons) were autonomously hauled in 2021 using Command for hauling.

In total, Command for hauling trucks have autonomously and safely hauled more than 4 billion tonnes (4.4 billion tons) of material since 2013. To date, trucks equipped with Caterpillar’s autonomous haulage system (AHS) have traveled more than 147 million km (91.3 million mi) with zero loss-time injuries, nearly the same distance as traveling from the Earth to the sun.

“Safety and sustainability continue to be top values in the mining industry. We are now entering our ninth year with zero loss-time injuries with Command for hauling, a testament to its safety record,” comments Marc Cameron, vice president, Caterpillar Resource Industries. “A recent five-year study by one of our customers autonomously hauling iron ore reported an 11% reduction in fuel usage – resulting in a 4300 tonne-per-year (4,740 TPY) CO2 emissions reduction – 11% increase in hourly production, 50% higher maximum truck travel speed, and 35% improved tire life.”

Autonomous trucks equipped with Command for hauling are operating at 18 mine sites by 10 companies across three continents. Commodities autonomously hauled include iron ore, oil sands, copper, coal and gold. Spanning the 190- to 360-tonne (210- to 400-ton) class sizes, the portfolio of Cat mining trucks capable of fully autonomous operation include the 789D, 793D, 793F, 797F and 794 AC with electric drive. Retrofit kits allow mining operations to expand Command for hauling to existing Cat mining trucks as well as other brands of trucks and loading equipment in their fleet.

“We continue to explore new avenues with Command for hauling to make strides toward the fully autonomous mine site and recently surpassed a major milestone of more than 500 autonomous trucks. Our previously announced collaboration with Newmont will introduce up to 16 autonomous trucks through 2023 at the company’s Cripple Creek and Victor mine in Colorado with plans to transition to haulage fleet electrification, supporting Newmont’s target of reducing greenhouse gas (GHG) emissions by more than 30%,” says Sean McGinnis, general manager for Cat Mining. “We currently have in progress high-altitude and new product introduction projects for the smaller 89-tonne (98.4-ton) size class. We have also expanded our Command system to Cat water trucks for haul road dust control at the mine.”

The Command hardware and technology is currently deployed on the Cat 789D autonomous water truck (AWT) at Rio Tinto’s Gudai-Darri mine in Australia, the world’s first AWT. Connected with Cat MineStar technology, Command for hauling on the 789D integrates the truck, tank and water delivery system (WDS). The Cat WDS delivers variable waterflow based on truck speed, and the system’s variable displacement pump automatically starts and stops when the truck slows or comes to a halt, preventing overwatering and poor traction at intersections.

More information on Cat Command for hauling trucks can be found by contacting a regional Cat dealer or visiting: https://www.cat.com

 

of

For the first time in mining history, trucks equipped with Cat® MineStar™ Command for hauling have autonomously moved more than 1 billion tonnes of material in less than a year.

View Full Size Image

Product & Service News

See the latest product and engine announcements from Caterpillar.

See the Latest News

 

# # #

 

CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

©2022 Caterpillar All Rights Reserved

 

 

Press Inquiries

Caterpillar Trade Press Media Representatives

Americas

Sharon Holling: Holling_Sharon_L@cat.com

Johanna Kelly: Kelly_Johanna_L@cat.com

Europe, Africa, Middle East

Francine Shore: Shore_Francine_M@cat.com

Reader Requests

www.cat.com/requestCatinfo

 

warning

Internet Explorer users may experience issues with certain features of our site.
Please try a current version of an alternate browser (i.e. Google Chrome, Microsoft Edge, Mozilla Firefox) for the full Cat.com experience.