Cat® 24 Motor Grader
Cat® 24 Motor Grader

Caterpillar celebrates production of 1,000th Cat® 24 Motor Grader

 

For Worldwide Release: September 2022 
Release Number: 677PR22

In 1995, Caterpillar introduced the Cat® 24 Motor Grader specifically designed to build and maintain haul roads at mining sites with ultra-class haul trucks. Now in its third generation, the Cat 24 offers 399- to 518-kW (535- to 694-hp) power, 61 950 kg (136,575 lb) weight, a 7.3-m (24-ft) moldboard with an 8.5-m (28-ft) moldboard option, and technology as standard to work wide haul roads efficiently. 

At a ceremony held on September 22, 2022, Caterpillar executives and motor grader production team members gathered in Decatur, Ill. to celebrate the production and sale of the 1,000th Cat 24 Motor Grader. The machine, destined for Australia, was sold by Cat dealer, WesTrac Pty Ltd, to Rio Tinto Pilbara Operations, located in Perth, Australia. During the event, Caterpillar team members heard from both WesTrac and Rio Tinto Iron Ore representatives, through videotaped comments, which conveyed the value the Cat 24 brings to the miner’s operation.

Commenting on the historic 1,000th Cat 24 milestone, Sam Vedhakumar Manoharan, vice president of product management, earthmoving, said: “The Cat 24 Motor Grader was and continues to be a game-changer for maintenance efficiency of the wide haul roads necessary for ultra-class trucks. We thank the many global mining operations and dedicated Cat dealers around the world for their loyalty to the Cat 24 grader.”

Today’s Cat 24 Motor Grader features more than 30% higher power, 13% more weight and a longer rebuild life than previous generations. It also offers an 8.5-m (28-ft) moldboard option and will soon feature a high-performance circle design for further improved reliability. The milestone machine includes a special 1,000th unit commemorative plate.

“For years, we have used Cat 24 Motor Graders to maintain our haul roads for our ultra-class trucks. The Cat 24 series offers a great combination of power, weight and blade width to support road maintenance coverage for our large mining fleet,” says Stephen Jones, Rio Tinto Iron Ore managing director of planning, integration and assets. “We are honored to receive the commemorative 1,000th 24 Motor Grader, and this represents the third generation we’ve used across our Pilbara mining operations.”

More information on the Cat 24 Motor Grader can be found by contacting a Cat dealer or visiting: https://www.cat.com/lmg. 

 

 

of

Caterpillar executives and motor grader production team members gathered in Decatur, Ill. to celebrate the production and sale of the 1,000th Cat 24 Motor Grader.

View Full Size Image
of

Caterpillar executives and motor grader production team members gathered in front of the 1,000th Cat 24 Motor Grader.

View Full Size Image

Product & Service News

See the latest product and engine announcements from Caterpillar.

See the Latest News

 

# # #

 

CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

©2022 Caterpillar All Rights Reserved 

 

 

Press Inquiries

Caterpillar Trade Press Media Representatives

Americas

Johanna Kelly: Kelly_Johanna_L@cat.com

Europe, Africa, Middle East

Francine Shore: Shore_Francine_M@cat.com

Reader Requests

www.cat.com/requestCatinfo

 

warning

Internet Explorer users may experience issues with certain features of our site.
Please try a current version of an alternate browser (i.e. Google Chrome, Microsoft Edge, Mozilla Firefox) for the full Cat.com experience.