New Cat® MineStar™ Reporting integrates MineStar
New Cat® MineStar™ Reporting integrates MineStar

New Cat® MineStar™ Reporting integrates MineStar and other vendor data into a single, unified interface

For Worldwide Release: July 2022
Release Number: 416PR22

Every piece of mining equipment constantly generates critical operating and production data that is used by Cat® MineStar™ products to enable miners to make better decisions. Historically, each MineStar capability – Fleet, Terrain, Health and others – has different reporting tools for this captured data.

Caterpillar launches its new Cat MineStar Reporting platform for MineStar Solutions, a powerful reporting and analytics product that can consolidate information from MineStar products. Currently, MineStar Reporting supports information from MineStar Fleet, Terrain, Health and Command for hauling. Support for MineStar Edge is currently underway, and all other products will soon be supported.

The easy-to-use reports and dashboards generated by MineStar Reporting are suitable for single or multiple mine sites and can efficiently work with other sources that aren't MineStar. Plus, it provides a single data layer for presentation and analysis regardless of MineStar version. A comprehensive set of reports and dashboards come standard with system installation.

Data collected from MineStar and other vendor technologies is unified by new MineStar Reporting into a comprehensive database that can be accessed simply and securely via a web browser. The flexible system allows users to create customized reports, so each person is equipped with the appropriate information, while automated email reports within the system ensures that the data is received at the right time.

Providing more graphical content for users, MineStar Reporting expands the breadth of reporting capabilities at the mine. The solution offers upgrades to connect to other mining data sources for more comprehensive analysis and summary of the whole picture, including spatial intelligence, process plant data and reconciliations. It provides product tracking with genesis tracing, stockpile management and reconciliations.  

The core reports and dashboards included with the new reporting platform allow users to quickly view and analyze mine site data. Standard production reporting encompasses management and movement summaries, benches mined, cycle details, truck production, and grade movement and summary. Equipment performance, time stats and delay overview, activity calendar, fleet timeline, and event details are covered in the time report. Users can quickly see drilling accuracy, hole list and drilling information using the standard drill report. A wide variety of maintenance reports are included with an expanded set using machine health data.   

Growing with the mine site’s use of automation, MineStar Reporting is scalable and future-proof. Using Connected Mine technology in partnership with Information Alignment, it simplifies reporting of currently gathered data while leaving space for future solutions when the mine is ready to adopt new technologies. With all data housed in a single location independent of one solution, valuable historical data is secure when updating or changing technology systems.

More information on new MineStar Reporting can be found by contacting a Cat dealer or visiting: https://www.cat.com/minestar-reporting

 

 

of

Currently, MineStar Reporting supports information from MineStar Fleet, Terrain, Health and Command for hauling.

View Full Size Image
of

The easy-to-use reports and dashboards generated by MineStar Reporting are suitable for single or multiple mine sites and can efficiently work with other sources that aren't MineStar.

View Full Size Image
of

Caterpillar launches its new Cat MineStar Reporting platform for MineStar Solutions, a powerful reporting and analytics product that can consolidate information from MineStar products.

View Full Size Image

Product & Service News

See the latest product and engine announcements from Caterpillar.

See the Latest News

 

# # #

 

CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

©2022 Caterpillar All Rights Reserved 

 

 

Press Inquiries

Caterpillar Trade Press Media Representatives

Americas

Sharon Holling: Holling_Sharon_L@cat.com

Johanna Kelly: Kelly_Johanna_L@cat.com

Europe, Africa, Middle East

Francine Shore: Shore_Francine_M@cat.com

Reader Requests

www.cat.com/requestCatinfo

 

warning

Internet Explorer users may experience issues with certain features of our site.
Please try a current version of an alternate browser (i.e. Google Chrome, Microsoft Edge, Mozilla Firefox) for the full Cat.com experience.