Meeting the power needs of India’s rapidly growing economy

Mumbai Chhatrapati Shivaji International Airport Terminal
Mumbai Chhatrapati Shivaji International Airport Terminal

Custom solution protects airport operations and ensures safety

Customer: Mumbai International Airport Private Limited (MIAL)

Location: Mumbai, India

Customer Business Issue: 24/7 electric power availability to maintain smooth operations and safety of planes for a newly opened international airport

Solution:

  • Six Cat® C175-16 standby diesel generator sets (3000 kVA each)
  • Three-year Operations & Maintenance (O&M) Contract
  • Product Support

Cat® Dealer: GMMCO Limited

of

6 sets of Cat C175-16 diesel generator sets

of

Chhatrapati Shivaji International Airport

of

Chhatrapati Shivaji International Airport

of

The new international terminal has a total area of 21,000 square meters and can accommodate 40 million passengers every year.

of

Chhatrapati Shivaji International Airport

POWER NEED

India’s financial capital, Mumbai, will have a new state-of-the-art terminal at the local Chhatrapati Shivaji International Airport, one of the fastest-growing and busiest airports on the Indian Subcontinent. Ranked the second busiest airport in India, its two older main terminals and twin intersecting runways are able to handle 36 flights every hour and this demand is projected to potentially increase exponentially in future, in line with the rapid economic growth happening in India.

To cater to the projected growth and improve the passenger handling capabilities of the airport, the operators of the airport, MIAL, embarked on a project to build a new, modern, Terminal Two passenger terminal complex on the site of the older Terminal Two building.

MIAL appointed India’s largest engineering and construction contractors, Larson & Toubro, to oversee the project. When completed, the new international terminal will cover 210,000 square meters of land area and will be able to handle up to 40 million passengers annually.

To support the smooth operation of the new terminal to ensure the safety of planes using the complex, MIAL could not afford to have power outages affect the new, modern passenger terminal.

Reliable power is also paramount in keeping the large space and the large number of passengers using the terminal cool, especially in the Indian summer heat, where temperatures can soar beyond 40 degrees Celsius.

SOLUTION

MIAL approached the local Cat dealer GMMCO Limited for assistance in designing a reliable backup power system for the new terminal building. The power requirements were challenging, it had to be reliable, provide enough power for the large terminal even on the hottest days and compact enough to be hidden away from the public-accessible areas of the building to preserve the aesthetics of the unique X-shaped terminal and comply with local Indian noise and emissions regulations, some of the strictest in the world.

To meet the challenge, GMMCO Limited designed a high power density, small footprint system comprising of six units of C175-16 diesel generator sets, each capable of providing 3,000 kVA of standby power in the event of grid power failure. The generator sets were also packaged locally into sound-attenuated containers to manage sound levels, and has customized intake and exhaust ducting fabricated locally to overcome the space restrictions without affecting the effectiveness of the generator sets.

RESULTS 

The Cat C175 gensets were installed in early 2013 and have been in operation to provide 24/7 standby power to ensure the smooth operations of the new airport international terminal. 

Supported by a three-year full Operations & Maintenance (O&M) contract with GMMCO Limited and an extended three-year warranty, the technically advanced Cat C175-16 generator sets are ready at all times to provide reliable power for MIAL to focus on maintaining safety and security of the passengers using the new terminal.”

Download the Power Profile

Featured products

  • Standby Rating
    3100(no fan)/3000 kVA
    3100(no fan)/3000 kVA
    Prime Power Rating
    2825(no fan)/2725 kVA
    2825(no fan)/2725 kVA
    Emissions/Fuel Strategy
    Low Fuel, Low Emissions
    Low Fuel, Low Emissions

    C175-16 (50 Hz)

    Producing reliable power from 2500 - 3100 kVA at 50 Hz, our 175-16 diesel generator sets are made to meet your mission critical, continuous, standby and prime applications. We've designed each to ISO 8528-5 transient response requirements and to accept 100% rated load in one step. The generator set is optimized for Low Fuel Consumption or Low Emissions.

    Learn More

Electric Power products

Any size or shape. In any regulatory environment. When you need power, Caterpillar is equal to the challenge. Our generators are used in a variety of applications.

View Electric Power products
electric power
electric power

Generator Set Sizing Calculator

Caterpillar Electric Power is excited to introduce you to our latest generator set sizing software, Cat® Electric Power SpecSizer.

Learn More
specsizer
specsizer

Commercial Business

You’re trusted to power the places people work and do it cost-effectively. Run uninterrupted power and reduce operating expenses. Install a Cat combined heat and power (CHP) system to simultaneously provide electricity for electrical loads and recover heat to warm facilities.

View Commercial Business Page
Commercial Business
Commercial Business

CAT® DEALERS MAKE THE DIFFERENCE

Your Cat dealer is committed to maximizing your success, helping you get the most out of your operations with site-level solutions, service and support.

CONNECT WITH YOUR DEALER TODAY
dealers
dealers