If you already have an existing account with another Cat App, you can use the same account to sign in here.
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
Some of the world’s toughest jobs are on mine sites. And if your dozer’s undercarriage isn’t up to the task, work will quickly grind to a halt. Your Cat® dozer undercarriage works and wears as a system, ensuring longer service life, increased uptime and lower costs.
Estimated read time: 3 minutes
Every Cat® mining dozer undercarriage is built to meet the rigorous demands of mine sites. The components are integrated with the machine and work together seamlessly. They’re field-tested for proven durability and reduced maintenance. That means maximum performance at the lowest cost — so you can move more materials, more efficiently.
The undercarriage represents on average 50% of your dozer’s owning and operating costs. Cat undercarriage components wear at a balanced rate, giving you longer life with predictable downtime and lower repair costs over the life of your bulldozer.
Designed based on years of field experience, a Cat general duty undercarriage is recommended for low-to-moderate impact applications. There’s also a heavy duty undercarriage system for hard rock applications with moderate-to-high impact levels. The components are interchangeable, which cuts the need for retrofitting and minimizes downtime.
When operated and maintained properly, Cat general duty undercarriages deliver value and performance. And the data from Cat dealers and customers proves it.
Let’s look at a diamond mine that had been buying a competitor undercarriage for their Cat D9 Dozers. To lower operating costs, the mine’s Cat dealer recommended the Cat general duty system with an undercarriage management program.
The customer conducted a trial on two of their D9 dozers, while the dealer monitored undercarriage performance. After collecting 6,000 hours of data, they saw that the Cat general duty undercarriage cost 10% lower per hour than the competitor undercarriage. That meant savings of more than $10,000 each year. The decision was simple for this diamond mine. They switched to Caterpillar.
The patented sleeve bearing track is standard on all D11 dozers and has more than 10 years of proven field performance. The sleeve bearing track eliminates galling, increasing track performance so your machines can keep working. It is designed to run at higher speeds while handling greater loads.
Bushings have a special coating to improve seal life, and the sleeve bearings are made of hardened steel. The track’s overall durability reduces maintenance costs and unscheduled downtime.
Available for D9-D11 dozers, the positive pin retention (PPR) track features specially machined links and pins that allow for the use of a metal retaining ring.
This ring fits in the groove between the pin and link, locking the joint to a predetermined specification. It prevents the outward movement (also known as end-play generation) of the links on the pin. The result is more uptime and increased productivity for your business.
The Cat Undercarriage Assurance Program gives you extended support for your undercarriage. Your Cat dealer will make sure you have service and support beyond the standard new machine or parts warranties. The program covers all major moving undercarriage components and can be customized to meet your needs.
Your Cat dealer has all the details about undercarriage configuration options and will help you make the right decision for your needs. Reach out today to learn more and take advantage of increased uptime, improved productivity and greater cost savings.
Get the most from your mining equipment with information about Customer Value Agreements, repair options and more.
Complete exchange axle rebuilds save time and reduce contamination risks on the mine site.
FIND OUT HOWYour Cat® dealer studies your undercarriage needs so you reap benefits on the mine site.
CONTACT YOUR DEALERWork with your Cat® dealer to keep your undercarriage maintenance and repairs on target.
SEE REPAIR OPTIONSReview mining repair indictors and find solutions to match your budget and timeline.
LEARN MORE TODAY