Machine Drive Power - Accurate Measurements

Cat Machine Drive Power: Save Time and Money with Accurate Measurements

Measure rolling resistance accurately and automatically—and move on to the next job confident you’ve met compaction requirements. That’s the advantage Cat® Machine Drive Power (MDP) delivers over conventional methods of measurement. It uses sensors to measure rolling resistance as the machine moves, then alerts operators when they’ve hit their targets.

Here are four ways MDP could make a big difference on your next project:

1. MORE COST SAVINGS

  • Taxpayers will benefit from extended life of public projects, such as roads, airports, levees and other infrastructure investments
  • Fewer required passes mean lower costs, which are likely to reduce bids
  • Realizing compaction problems during the job allows you to make adjustments immediately, avoiding rework

2. FEWER PASSES

  • Reduce fuel burn
  • Use labor more efficiently
  • Use machinery more productively
  • Meet project deadlines

3. BETTER MONITORING

  • In-cab display provides operator with real-time feedback
  • Stiffness can be monitored both in the cab and remotely—at a computer, on an iPad or over a smartphone if VisionLink is being used
  • Also with VisionLink usage, state and federal inspectors can remotely monitor a project

4. INCREASED DATA COLLECTION

  • Does not measure as deeply as accelerometer-based systems; monitors closer to the depth of typical lift
  • Operators produce data on 100% of the surface, compared with 1% using traditional portable testing devices/methods with mapping
  • Works well on all types of soils: fines, granular and cohesive
  • Measures with the vibe system on or off; can handle proof rolling
  • Performs on smooth drums, padfoot drums or smooth drums equipped with shell kits

IMPROVE WITH CAT PAVING TECHNOLOGY

Cat Paving technology pays for itself. Get more insight into your equipment and operations than ever before.

GET CONNECTED
CAT PAVING TECHNOLOGY

STAY CURRENT WITH ENEWS

We send industry knowledge, useful tips and special offers right to your inbox.

Sign Up

RELATED ARTICLES

You’re here to get ideas to grow your business. Read on for machine insights and expert tips and tricks to get more out of every job.