General duty or multi-purpose? Clean-up or ditch cleaning? Digging or grading? When it comes to selecting buckets for your excavator or loader, the options can seem endless. It’s tempting just to pick the biggest one that fits your machine and hope for the best. But making the wrong choice can have dire consequences — reducing your productivity, increasing your fuel burn and causing premature wear. That’s why it pays to go into the bucket selection process with a strategy. Start by asking these three questions:
The density of the material you’re working with plays perhaps the biggest role in bucket selection. It’s a good idea to make your choice based on the heaviest material you handle most of the time — keeping in mind that with very heavy, hard-to-get-through material, you might not be able to load a large bucket to full capacity. In those conditions, a smaller bucket may out-dig a larger one by allowing your machine to cycle faster.
Here are a few common bucket options matched to material types. This is just a small sampling of what’s available, so be sure to talk to your equipment dealer about specialty options available that may be better suited for your jobs.
A bigger bucket means more production, right? Not necessarily. Any short-term gains likely will get wiped out by repairs and downtime. That’s because using a bucket that pushes your machine over the recommended capacity limit — even by just a few percentage points — accelerates wear, reduces component life and risks unplanned failure.
The key to maximizing productivity is this: First, consider the capacity of the machine you’re loading. Next, determine how many loads you need to move each day. Then, select the bucket size that gives you the ideal pass match. In fact, it may make sense to determine your bucket size first, then select the machine that can accommodate it — not the other way around.
You pay close attention to features and options when you buy a machine — be sure to do the same when you choose a bucket. (It’s doing the hard work on the job, after all.) A bucket with qualities like these will help you get more done in less time for less cost:
More choices mean more questions.
Equipment manufacturers are developing new buckets and bucket options all the time to increase productivity and life in every application, so consider these three questions the first of many you’ll want to ask your dealer before you make a final bucket selection. Still, you can’t go wrong if you start with these basics. Looking for more guidance? Check out these tips for matching bucket type and material.
You’re here to get ideas to grow your business. Read on for machine insights and expert tips and tricks to get more out of every job.
When to comes to selecting a bucket for your heavy equipment, the wrong decision could increase your costs by 10 to 20%–and cut productivity at the same time.
Learn MoreHow do you optimize Wheel Loader Performance and Productivity? Take a look.
Learn MoreMaterial Density determines bucket and machine choices. Construction companies often select the size of machine they believe is required and equip it with a standard bucket, but this approach might short change productivity.
Learn MoreWe dive into the latest nursery tools for landscaping and agriculture businesses that might help you be more productive.
Learn More