If you already have an existing account with another Cat App, you can use the same account to sign in here.
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
There’s a simple way for operators of various skill levels to push light and heavy loads more effectively. Get the scoop on Steer Assist.
Bad news: The shortage of skilled machine operators persists. Good news: Equipment manufacturers are taking steps to help contractors deal with the issue from inside the cab — incorporating assist features that make the work easier.
These operator “helpers” automate blade, bucket, steering and other machine functions. This enables newer operators to work at productivity levels closer to their veteran counterparts. Seasoned operators benefit, too. Reduced effort and fatigue may allow them to stay on the job for longer.
Let’s take a closer look at one of the aides available specifically for dozer operators: Steer Assist.
Cat® Steer Assist for Dozers automates multiple steering functions: track steering (for light and heavy loads) and blade tilt steering (for heavier loads). It automatically maintains straight line travel — ideal when working on slopes but helpful on flat ground, too. And it works in both forward and reverse. Just start your pass and Steer Assist does the rest.
There’s also a 3D version that automatically follows guidance lines from both 3D digital site design files and infield designs. Steer Assist 3D helps operators more accurately cut and spread material to an edge, toe, crown, etc. so they can achieve precise pass-to-pass overlap in fewer passes. That saves time and fuel.
Both the standard and 3D versions of Steer Assist can reduce operator inputs by up to 75% when maintaining straight travel on side slopes.
Operation is simple. Just turn on Steer Assist using the dozer monitor. Then shift into forward or reverse, steer to the desired heading and release steering command to maintain it. Steer Assist 3D requires first loading the 3D digital site design file and selecting the horizontal guidance line. Then shift into forward, engage AUTO mode on the joystick, move the blade tip within the capture range and release steering command.
Operators can take manual control of dozer steering or the blade anytime to override the system. When they’re not giving a manual command, Steer Assist takes control once again.
Want to boost dozing productivity even further? Use Steer Assist in conjunction with other Cat dozer assist features like AutoCarry, Traction Control and Grade with 3D.
Check out these videos of Steer Assist and Steer Assist 3D in action, then ask your local Cat dealer for an in-person demo. Steer Assist works on all D5 and D7 dozers, plus D6 and D6 XE models with serial numbers 1000 and above. The standard version is included with ARO with Assist — no GNSS signal or additional hardware required. Steer Assist 3D comes as part of the factory-installed Grade with 3D package. Your dealer can walk you through the details about upgrades and retrofits, too.
You’re here to get ideas to grow your business. Read on for machine insights and expert tips and tricks to get more out of every job.
The benefits of community service for a business are about much more than the bottom line. More and more these days, your customers are actively searching for companies that make social responsibility a part of their values. It's also just the right thing to do.
Learn MoreRyan Goodfellow, owner of Rock Structures, talks about his strategies on recruiting and retaining construction crews as well as advice for new operators.
Learn MoreWe dive into the latest nursery tools for landscaping and agriculture businesses that might help you be more productive.
Learn MoreFrom E-Fence to Indicate features, check out the new mini excavator technology, helping to make your time in the cab more efficient.
Learn More