Excavators offer your worksites a tremendous range of power and versatility. Because there are so many machines and options to choose from, it can be a complex process to determine what model will deliver the most productivity at the lowest operating cost. With today’s tight bidding climate, it only makes sense to “dig in” to your decision-making process and do everything you can to increase your profitability. Use these tips as a solid starting point:
Mini or compact excavators:
(Approximate weight: up to 13,000 lbs./6 metric tons)
Midi excavators:
(Approximate weight: 15,400 lbs./7 metric tons – 22,000 lbs./10 metric tons)
Standard excavators:
(Approximate weight: approximately 22,000 lbs./10 metric tons – 99,200 lbs./45 metric tons)
Large excavators:
(Weight: more than 99,200 lbs./45 metric tons)
Every time you estimate a job, you use the volumes of dirt you need to move, grade, slope or compact as a basis for costs. But it’s not often that you compare multiple jobs based on the digging depth, reach, breakout force, bucket capacity and lift capacities. So before you shop excavators, consider these questions:
BUDGET
WORKSITE CONDITIONS
DIGGING DEPTH & REACH
LIFTING CAPACITY
BUCKET CAPACITY
COUNTERWEIGHT
HYDRAULIC ATTACHMENTS
TRANSPORTATION
TECHNOLOGY
Finding the right excavator requires research and running the numbers. Once you know what targets you want the excavator to hit, then it’s time to talk experts you trust and to demo some machines. You may be able to rent the models you’re interested in and try them on several jobs, or you can talk to your local dealers. The most important thing is to measure all the options against what will add the most to your business.
Your Cat® dealer can help you figure out what excavator works best for you, talk to them today.
You’re here to get ideas to grow your business. Read on for machine insights and expert tips and tricks to get more out of every job.
CONEXPO-CON/AGG 2020 is well underway, and Cat® technology is one of the main events.
Learn MoreSerene waterfalls. Babbling brooks. Tranquil ponds. And the quiet purr of Cat® equipment in the distance … sounds like a little piece of paradise, right? That’s just what we found when we arrived at Pondemonium 2019 a few weeks ago with our In The Trenches Tour featuring Next Generation Cat Mini Excavators. This experience was like no other landscaping event in world. And we couldn’t wait to share a recap with you in the latest “On The Level” blog. If you don’t already love your job, you will after reading this!
Learn MorePennsylvania-based hardscaper, Guimento and Son Hardscapes LLC, has been using Cat® machines to help them get the job done from day one. After experiencing total numbness in his hands while operating in cold weather conditions and ultimately, a Type 2 diabetes diagnosis, John Guimento knew he needed a solution. The climate-controlled cab of the Next Generation Cat 302 CR Mini Excavator was the answer.
Learn MoreWe caught up with Tom Gardocki of The Dirt Ninja to learn about his top construction attachments for excavating and how they can improve your efficiency.
Learn More