Here’s a pretty startling statistic—in the next year, the off-highway engine market will consume about 20 million gallons of Diesel Exhaust Fluid (DEF). In the next five years that number is projected to rise to 260 million gallons. That’s a lot of equipment running with DEF. DEF does require special attention in its use and storage, so here’s a quick hit list to help you and your crew handle it effectively.
You should always use DEF that meets OEM specifications for your equipment.
DEF used in Cat® SCR systems must meet the requirements outlined in the International Organization for Standardization (ISO) standard 22241-1. ISO 22241-1 requirements are met by many brands of DEF, including those that carry the AdBlue or API certifications.
The DEF tank on Cat machines has a 1:1 fill rate with the fuel tank. If fuel is added, DEF needs to be added. The DEF fill cap is an industry standard blue and easily identifiable.
DEF will start to freeze at 12 degrees Fahrenheit (-11°C), so you’ll want to store it in a conditioned space if possible.
DEF will expand when frozen, just like water. Approved containers are designed to handle the expansion and contraction, just like the DEF tanks on your equipment. Freezing does not change the effectiveness of the fluid.
The ideal storage temperature for DEF is between 15ºF and 77ºF (-9ºC and 25ºC). It should not be exposed to direct sunlight for long periods of time as the urea will decompose.
Refer to ISO 22241-3 for further information regarding DEF handling, transportation and storage.
Contamination could cause your system to use more DEF than it should, degrade components and even lead to emissions system failure. If contamination damages the catalyst in your SCR system, it could void the warranty. The catalysts in SCR systems use rare metals and replacing one can cost as much as $15,000. When refilling the DEF tank, clean thoroughly around the fill neck and the dispensing nozzle every time. Most DEF tanks have only sediment filters and lack the kind of high-efficiency filtration common to diesel fuel and air systems.
Transfer containers should be avoided. If a container must be used, use it ONLY for DEF.
If operators run machines according to manufacturer’s recommendations, there should be no problems with DEF. However, it is good practice to pay close attention to idle time. Too much idling of new emissions-compliant machines can build up soot in their diesel particulate filters, requiring more frequent regens. Excessive idling can also cause the DEF to crystalize in the injectors which can cause even more problems. Making sure that operators keep idle time to a minimum also saves fuel and reduces maintenance costs.
You’re here to get ideas to grow your business. Read on for machine insights and expert tips and tricks to get more out of every job.
Keep your farm equipment up and running with these skid steer maintenance tips.
Learn MoreLearn how rust damage prevention helps preserve your machine’s resale value and performance.
Learn MoreKeeping machines running smoothly in your snow and ice removal operation is key to keeping costs down. Learn more about how Cat® Customer Value Agreements (CVAs) can benefit you.
Learn MoreShopping for the right tools for your business? We explore the most important things to know before you buy snow removal attachments.
Learn More