Proven Reliable Energy Efficiency

red stripe
red stripe

Red Stripe Lager has been Using Waste Heat to Reduce Costs

 

Customer: Red Stripe

Location: Kingston, Jamaica

Customer Business Issue: Reducing electricity costs with a reliable, energy-efficient solution in a CHP system

Solution: Two Cat® CG170-16 gas engines

Cat® Dealer: IMCA Jamaica Limited

of

Harvest Power works with a variety of municipalities and private haulers to provide simple solutions for food waste recycling.

POWER NEED

Founded in 1928, Red Stripe is a pale lager proudly brewed in Kingston, Jamaica. Serving Caricom, Canada, the UK, the EU and the U.S., this growing brand became part of the Heineken family in 2015.

Prior to 2013, electricity costs at Red Stripe were high at the plant; a plan was created to save on electricity costs, reduce their carbon footprint and become more energy efficient.

SOLUTION

In 2014, Red Stripe installed a CHP plant as part of this plan. CHP plants simultaneously generate heat and electricity during the same process, therefore increasing effectiveness and reducing the amount of fuel used in operation. By using heat that is wasted during the conventional production of electricity, the CHP plant offers significant environmental benefits. The system requires less fuel to produce the same amount of energy, which reduces greenhouse gas emissions such as carbon dioxide.

“CHP is a highly efficient way to produce energy and the technology is both proven and very reliable in achieving significant cost savings, environmental benefits, enhanced energy security and overall efficiency in excess of 80%,” said Neil Grant, engineering and maintenance manager at Red Stripe.

Red Stripe’s CHP system was designed by Caterpillar and included two Cat CG170-16 gas engines as the main components. These provided the average power needs for Red Stripe plant, as well as steam and thermal energy.

RESULTS

The two Cat engines supplied a combined 2,060 kW, which is 80% of Red Stripe’s requirement.

However, Red Stripe encountered a failure with an engine within the CHP plant. IMCA, the local Cat dealer in Kingston, Jamaica, supported the plant by providing spare parts and the necessary service to fix the engine within the established timeline and the continuation of the cost saving projections.

“By engaging IMCA to do the repairs on the engine for us, we noticed a few things,” said Grant. “First, the service was approximately 20-30% cheaper than the overseas supplier. Second, the capability, professionalism and responsiveness made IMCA easy to work with. It was more of a partnership, and that made a world of difference in the relationship between IMCA and Red Stripe.”

The repair to the CHP plant resulted in savings of approximately 5 million Jamaican dollars (40 thousand U.S. dollars) per month in electricity costs.

“This has resulted in IMCA becoming our first-choice provider for the service of our engines,” noted Grant. “We now have a renewed confidence in the customer service and support from IMCA as our Cat dealer.”

Download the Power Profile

 

Featured Products

  • Continuous Rating
    2519 / 2500 ekW @ 1.0pf
    2519 / 2500 ekW @ 1.0pf
    Fuel Type
    Natural Gas, Hydrogen Blend (up to 25%)
    Natural Gas, Hydrogen Blend (up to 25%)
    Maximum Electrical Efficiency
    45.30%
    45.30%

    G3520H

    From natural gas to biogas, coal mine gases, or hydrogen fuel blends to support combined heat and power (CHP), emergency power, and local grid support applications, Caterpillar has a wide range of reliable gas power solutions.

    Learn More

Electric Power products

Any size or shape. In any regulatory environment. When you need power, Caterpillar is equal to the challenge. Our generators are used in a variety of applications.

View Electric Power products
electric power
electric power

Generator Set Sizing Calculators

Cat Electric Power now has two tools available for sizing gensets in any application. 

Size Now
genset sizing
genset sizing

Manufacturing

When your lines aren't moving, you're not making money. You need power that will keep you in production and keep you efficient. Cat standby generator sets run with low owning and operating costs. We’re helping you maximize profit by minimizing electrical expenses.

View Manufacturing Page
manufacturing
manufacturing

CAT DEALERS MAKE THE DIFFERENCE

Your Cat dealer is committed to maximizing your success, helping you get the most out of your operations with site-level solutions, service and support.

CONNECT WITH YOUR DEALER TODAY
dealers
dealers