Electric fleets and natural gas-powered solutions are transforming wellsite services. As mobile power generation technology evolves, the oil and gas industry is exploring how to erect different types of microgrids that can be customized to their unique operational needs.
According to Evolution Well Services President and CEO Steven Anderson, electrifying hydraulic fracturing and other energy-intensive completions operations can contribute positive economic, operational, safety and climate-related benefits to the oil and gas industry1. These include improved safety for personnel and equipment, reduced crew size, lower fuel costs and decreased greenhouse gas (GHG) emissions associated with oilfield operations.
As a next-generation pressure pumping company, Evolution utilizes Caterpillar Oil & Gas technologies to empower and energize oilfield services, bringing ultra-mobile power generation solutions directly to the wellsite. These mobile power generation systems, or microgrids, can operate in a much smaller geography to produce power where and when it’s needed. With oil and gas operations requiring a steady power source 24/7, utilizing local stand-alone microgrids is helping to revolutionize oilfield electrification and technology solutions.
A mobile microgrid provides on-site electric power directly to the loads, eliminating the need for distribution infrastructure from a centralized power generation location. To that end, microgrids are self-sufficient distributed energy resources (DERs) that are capable of generating the required power for on-site demand. Two of the most common types of DERs include natural gas-fueled gensets and turbines. These DERs operate in an island mode (off-grid) or interconnected with the utility provider on location (grid-connected microgrids).
From a technology perspective, one of the most pivotal technology shifts in the oilfield within the past two years is the ability to tap into utility power to supplement the power needed to operate a wellsite. The impact of this approach could be significant as supplementing a site with utility power can reduce the number of gensets required, helping preserve capital while lowering operating costs as well as related GHG emissions.
Given the high-availability operating requirements of the oil and gas business, it’s important to know that the core functionality of these innovations is field-proven.
Modern microgrids can be successfully implemented in the oilfield to help companies achieve operational and climate-related targets without compromising performance. A Permian operator’s experience demonstrates the benefits that are possible with an optimal microgrid approach2.
An operator desired to implement a grid-connected microgrid to power its wellsite as part of an e-frac application to support two goals: reduce fuel consumption costs and lower GHG emissions. The grid-connected microgrid enabled the operator to use six gas-fueled gensets on-site rather than 10 units while reserving one unit on standby in the event of any fluctuations. The power management system allowed the operator to reduce the need for on-site power generation by 40% by replacing that power demand with grid power. Additionally, site operations were not affected by blackouts, which were prevented by the coordination of protection relays in alignment with load variations.
Grid-connected microgrids are the optimal approach to advance electrifying the oilfield, as such configurations enable companies to leverage the maximum amount of power a utility can provide and supplement the rest with on-site power generation. This approach also offers oilfield companies the option to export power to the grid if needed. While grid-connected microgrids are highly desirable, project suitability is governed not only by grid accessibility but also the grid’s power capability for a specific site. With current strains on the electrical grid and the tremendous amount of power oilfield sites require, it’s important to understand if the amount of power a utility can provide will be suitable.
Electrifying oil and gas operations are driving safety, efficiency and reliability improvements in the oilfield, according to Anderson. As part of the industry’s dynamic mix of power generation solutions, electrification can support growing demand which serves to energize the future of oil and gas applications.
While the upfront costs to convert equipment may be capital intensive, these systems and electrical components are long-lasting and reliable, ultimately returning the investment in the long run.
As the oil and gas industry continues to evolve, electrification is expected to be a major contributor to the sector’s change. Developing necessary infrastructure and improving power generation technology are essential to support advanced electrification options to realize reduced costs, potentially lower GHG emissions and enhanced operational efficiency.
1. Cat.com. The Energy Pipeline Podcast. Electrification in Oil and Gas. https://www.cat.com/en_US/campaigns/awareness/the-energy-pipeline/electrification-in-oil-and-gas.html
2. Caterpillar Oil & Gas. 2024 ATCE #220763. A Permian Microgrid Case Study – Keys to Successful Implementations.
Jordan Yates & Bill Jenson interview Steven Anderson, President & Chief Executive Officer at Evolution Well Services on the emerging trend of electrification in the oilfield and its role in driving sustainability.
Learn MoreCat Smart Engine Management System efficiently manages the number of engines required to satisfy performance needs.
Learn MoreAs fuel is always one of the greatest expenses in the oilfield, technological advances that drive greater efficiencies are top of mind for E&P s and drilling operators. Newly available electrification and optimization technologies lower fuel consumption and related greenhouse gas emissions while maintaining on-site reliability and durability.
Learn More