Sitewide solutions drive operational efficiency and customer satisfaction for Trican
Trican Well Service Ltd.
Well Services
Comprehensive sitewide solution encompassing DGB T4, transmission, high-performance frac pump and pump consumables as well as frac iron
Canada
Trican Well Service Ltd. takes advantage of Caterpillar’s advanced equipment and technology to enhance performance and fuel cost savings.
As a full-service provider of cementing, coil tubing and fracturing services, Trican Well Service Ltd. is committed to investing in new and integrated solutions that can help increase operational efficiency and support climate-related objectives. The company strives to pump more each day without increasing cost and is proactively using natural gas to curb diesel consumption and reduce greenhouse gas (GHG) emissions.
Fuel efficiency and on-site availability are especially important given the remote locations and brutal below-zero temperatures in British Columbia and Alberta where the company operates. With these challenges in mind, Caterpillar Oil & Gas has enabled Trican to continuously modernize operations and embrace alternative fuel sources while maintaining reliable performance in harsh operating conditions.
To improve operational efficiencies, Trican required a comprehensive site solution that would maximize uptime, optimize wellsite performance and displace higher-cost diesel. The company collaborated with Caterpillar Oil & Gas to develop an advanced comprehensive solution aligned with the company’s full-service approach to the oilfield.
For more than 30 years, Trican has trusted Cat and SPM technologies and services to support pressure pumping operations in challenging conditions and implement technology upgrades that support climate-related targets.
Trican was the first to trial the Cat 3512E Dynamic Gas Blending™ (DGB) engine in its region and has since deployed more than 75 3512E DGB T4 engines across its fleet, making it the largest lower-emissions fracturing fleet in Canada.
“As the cost of natural gas is significantly less than diesel, Cat DGB technology helps us substantially lower fuel spend, ensures a ready fuel source on-site and supports our transition to natural gas as the company’s primary fuel,” said Trican’s Vice President, Fracturing, Jim Rukin.
“DGB technology is fueling growth without the cost,” added Ty Sutherland, Hydraulic Fracturing Division Manager for Trican. “We used to bring 30,000 liters of fuel to a site each day, and now we do that every three days. We’ve also seen increased pump times and efficiency from integrating our Cat engines and SPM pumping technologies.”
In addition to the Cat 3512E DGB T4 engine, Trican also operates the Cat TH55-E90 transmission in its pressure pumping operations. It’s the company’s transmission of choice due to its smaller footprint and ability to run 20,000 to 25,000 hours before requiring an overhaul. The well services leader also uses several SPM technologies in the field including the QEM 3000 pump. To further enhance operational efficiency from pump to wellhead, the company was the first in Canada to utilize the SPM Large Bore to eliminate excess iron and reduce rig-up time. Trican also uses the high-performance pump consumable SPM EdgeX carbide seats throughout its pump portfolio for extended service life, reduced NPT and lower operating costs.
Trican continues to experience long-term benefits resulting from the application of both Cat and SPM innovations working seamlessly as a total site solution for consistent durability, efficiency and longevity in the field.
Cat DGB technology has delivered an average diesel displacement rate of up to 70%, with up to 85% peak diesel displacement under certain operating conditions. This important fuel flexibility has helped Trican decrease its diesel consumption and operating costs in addition to supporting the company’s GHG emissions reduction goals. The DGB engine also enables the well services company to operate near continuous duty under the harshest operating conditions. Combined with 3,000-horsepower capacity QEM pumps capable of withstanding high pressures ranging from 12,000 to 13,000 psi, operators have extreme confidence in Trican’s systematic approach to achieving operational excellence.
Keeping pace with the oil and gas industry’s changes requires a relentless commitment to innovation and continuous improvement. Utilizing solutions that are purpose-built for demanding conditions provides the rugged durability and operational efficiency Trican requires to continuously optimize costs and support climate-related objectives.
“Using a broad range of Cat and SPM solutions enables us to lower fuel consumption and costs without sacrificing high performance, so we can continue to meet growing global energy demands as the industry evolves,” said Trican Chief Operating Officer Todd Thue.
1. Trican Well Services. https://tricanwellservice.com/trican-deploys-canadas-first-low-emissions-fracturing-fleet/