If you already have an existing account with another Cat App, you can use the same account to sign in here.
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
Houston, TX – Offshore customers operating in potentially hazardous conditions now have access to a flexible rental solution from Caterpillar—a new hazardous location generator set certified to NEC 500 Class I Division 2 standards. Offering 994 bKW at 1800 rpm and 874 bkW at 1500 rpm, the Cat® C32 Petroleum CI/D2 Hazardous Location generator set is primarily intended for customers seeking an interim power solution that addresses stringent safety requirements.
“It’s a certified solution from the factory, built to the customer’s specifications,” said Scott Roberts, oil and gas offshore marketing manager for Caterpillar. “Because these units are designed to be dealer-owned, customers can use them on an as-needed basis. Wherever in the world a customer’s rig happens to be, a Cat dealer is nearby who can provide a temporary power solution.”
The C32 Petroleum CI/D2’s key features include a wet exhaust manifold and an ATEX-compliant wiring harness that prevent sparks and ignition of flammable gas. The Electronic Control Module harnessing is protected with robust guarding and connections sheathed in flame-retardant material. All cabling is enclosed in airtight sheaths, and an optional air shut-off automatically shuts down the engine to prevent gas from entering. The generator set meets IMO II emissions requirements. “Safety is the top concern of shipyards and rig owners these days,” Roberts said. “The C32 CI/D2 is one way Caterpillar and our dealers can help address that issue.”
As a rental generator set, the C32 CI/D2 also helps customers save time and expense.
“There’s nothing they have to do other than put in fuel and water and hook it up,” Roberts said. “Our customers don’t have to spend any capital on this unit—just rent it, put it on their rig, use it till they’re done and then give it back to the dealer.”
The C32 Petroleum CI/D2 Hazardous Location generator set is available now for order through the Cat dealer network. For more information on this product and other solutions for the oil and gas industry, follow Caterpillar Oil & Gas on Facebook (http://www.facebook.com/caterpillaroilandgas) and Twitter (http://www.twitter.com/catoilandgas) or visit www.cat.com/.
# # #
Caterpillar Oil & Gas, Caterpillar Inc.’s oil and gas division with headquarters in Houston, Texas, consolidates all the sales and service activities for Cat oil and gas power solutions. Since the 1930s, Caterpillar has manufactured engines for the oilfield and today provides premier power solutions with outputs from 31 to 16,000 kW. The sales and service network includes more than 2,100 dealer locations world-wide dedicated to support customers in the drilling, production, well service and gas compression segments. More information is available at: http://www.catoilandgasinfo.com
For 90 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent. Customers turn to Caterpillar to help them develop infrastructure, energy and natural resource assets. With 2014 sales and revenues of $55.184 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. The company principally operates through its three product segments - Resource Industries, Construction Industries and Energy & Transportation - and also provides financing and related services through its Financial Products segment. For more information, visit caterpillar.com. To connect with us on social media, visit caterpillar.com/social-media.
More information is available at www.cat.com.
Press Inquiries |
Jenna Janik Marcoux Phone: +1 713 895 1449 Cell: +1 979 541 9997 Marcoux_Jenna_J@cat.com |