If you already have an existing account with another Cat App, you can use the same account to sign in here.
One Account. All of Cat.
If you already have an existing account with another Cat App, you can use the same account to sign in here.
Account Information
Site Settings
Security Settings
For Worldwide Release: September 2024
IRVING, TEXAS – Caterpillar Inc. today announced that Deromedi Carrières et Matériaux is using a combined heat and power (CHP) solution from Cat® dealer Eneria France to support its sustainability and energy optimization goals at its limestone quarry in Ciez, France.
Designed, installed and commissioned by the Eneria team, the containerized system features a Cat CG170-12 gas generator set configured to operate on propane fuel already used on site. The solution was selected for its fuel flexibility, enabling it to operate on renewable gas fuels such as bio-propane as they become commercially available.
The system provides 850 kW of power for quarry operations and 605 kW of heat energy for drying processes while reducing NOx emissions to less than half of the TA Luft standard (under 100 mg/Nm3 at 15% oxygen).
Additionally, Eneria France supports long-term performance expectations and return on investment through an annual Customer Value Agreement (CVA), which includes regular maintenance at scheduled intervals as well as around-the-clock, on-demand technical support.
“At Deromedi, we are strongly committed to limiting environmental impacts at every level of our operations,” said Christophe Campos, Ciez site manager for Deromedi. “Eneria France has delivered a highly efficient CHP solution that supports our responsible approach while reducing energy costs.”
Cogeneration Capabilities from Caterpillar
Facilities can reduce operating costs by implementing a Cat CHP system or a combined cooling, heat and power (CCHP) system. Most Cat gas-fueled engines can be configured with a CHP or CCHP system to simultaneously generate power for electrical loads while capturing waste heat that can be repurposed as thermal energy for facility processes or heating, ventilation, and cooling requirements.
While the combination of grid power and traditional boilers for thermal energy offers less than 50% energy efficiency, CHP and CCHP systems from Caterpillar can provide total energy efficiencies of up to 90%. This allows customers to save on energy spending, provide autonomy of supply and reduce emissions.
Cat CHP and CCHP systems can deliver a rapid return on investment for a wide range of industrial and commercial facilities, such as manufacturing plants, refineries, regional district heating plants, resorts, shopping malls, high-rise office buildings, universities, data centers, and hospitals.
“Caterpillar’s CHP systems are proven solutions for helping enterprises maximize the return on their energy purchases while supporting their commitments to a lower carbon future,” said Sven Buehler, territory manager for gas product sales at Caterpillar.
For more information, visit www.cat.com/chp.
###
About Deromedi Carrières et Matériaux
With 40 years of experience in quarrying, Deromedi provides mineral fillers, aggregates and concrete for wide range of industry segments. The company produces 1.5 million tonnes of materials annually at six sites located throughout France. Visit https://www.deromedicarrieres.fr/.
About Caterpillar
With 2023 sales and revenues of $67.1 billion, Caterpillar Inc. is the world’s leading manufacturer of construction and mining equipment, off-highway diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. For 100 years, we’ve been helping customers build a better, more sustainable world and are committed and contributing to a reduced-carbon future. Our innovative products and services, backed by our global dealer network, provide exceptional value that helps customers succeed. Caterpillar does business on every continent, principally operating through three primary segments – Construction Industries, Resource Industries and Energy & Transportation – and providing financing and related services through our Financial Products segment. Visit us at caterpillar.com or join the conversation on our social media channels.
© 2024 Caterpillar. All Rights Reserved. CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.
Press Inquiries
Bob Chase
Gelia
Tel: +1 716-629-3230
bchase@gelia.com
Hazel Salmon
Caterpillar Inc.
SALMOH@cat.com