If you already have an existing account with another Cat App, you can use the same account to sign in here.
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
Cat Dynamic Gas Blending™ Retrofit Kit Provides Customer with Stellar Substitution Rate
Houston, Texas – Cat Dynamic Gas Blending™ (DGB) technology has delivered in China. Two® Cat DGB retrofit kits were installed on 2x 3512B generator sets, each rated at 1.2 MW @ 1500 rpm for a gas supplier operating in the Tarim Oilfield in China. The kits are achieving a substitution rate of sixty-percent for the majority of the load range, a significant accomplishment in the region. Cat dealer China Engineers Limited led Caterpillar efforts on the sale, commissioning and continued product support.
“For the customer, the primary benefit of the DGB solution was the substitution rate achieved during a comprehensive testing time, delivering unmatched performance in the region,” Hon Meng Lim, Caterpillar Oil & Gas Asia Pacific product support manager stated. “The generator sets delivered the same transient load response operating in dual fuel mode as they did in diesel mode without any unexpected shut-downs or load-sharing issues.”
Dynamic Gas Blending is Caterpillar’s dual fuel technology for land drilling, production and well stimulation applications. Originally introduced to the market in 2012, the Cat DGB retrofit kits have become the industry’s leading dual fuel solution, operating in oilfields around the world. Along with the benefit of realizing significant fuel cost savings by substituting diesel fuel with natural gas, there are several other key features of the Cat DGB system that make it a winning solution for the oilfield. Operators can run the system with confidence on CNG, LNG, and a wide range of field gas. The system automatically adjusts to changes in gas quality without the need to perform any recalibration or adjustments to the system during or between jobs.
The Cat DGB kit for land drilling and production also includes an EMCP 4.4 panel as standard equipment. In addition to handling routine generator functions such as paralleling and load sharing, the EMCP 4.4 can automatically start and stop generators based on overall rig power demand. The kit is backed by a full factory warranty and designed to be easily ordered through the Cat dealer network. “For our customers, it is convenient for us to service as a single-source supplier with flexible, fully-supported power solutions for their operations,” Lim noted. “The importance of a factory-issued warranty has undoubtedly contributed to the DGB kits popularity in China.”
Visit Caterpillar Oil & Gas at the Offshore Technology Conference, held in Houston, Texas, May 4th – 7thth at booth #3341. For up to the minute information on Caterpillar Oil & Gas, follow us on Facebook: http://www.facebook.com/caterpillaroilandgas & Twitter: http://www.twitter.com/catoilandgas. For more information on the comprehensive gas compression solutions Caterpillar offers, please visit catoilandgasinfo.com .
# # #
Caterpillar Oil & Gas, Caterpillar Inc.’s oil and gas division with headquarters in Houston, Texas, consolidates all the sales and service activities for Cat oil and gas power solutions. Since the 1930s, Caterpillar has manufactured engines for the oilfield and today provides premier power solutions with outputs from 31 to 16,000 kW. The sales and service network includes more than 2,100 dealer locations world-wide dedicated to support customers in the drilling, production, well service and gas compression segments. More information is available at: http://www.catoilandgasinfo.com
For nearly 90 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent. Customers turn to Caterpillar to help them develop infrastructure, energy and natural resource assets. With 2014 sales and revenues of $55.184 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. The company principally operates through its three product segments - Resource Industries, Construction Industries and Energy & Transportation - and also provides financing and related services through its Financial Products segment. For more information, visit caterpillar.com. To connect with us on social media, visit caterpillar.com/social-media.
More information is available at www.cat.com.
Press Inquiries |
Caterpillar Oil & Gas Press Relations: Jenna Janik Marcoux Tel: +1.713.895.1449 Marcoux_Jenna_J@cat.com |