Caterpillar Extends Industry Leadership in High Power Density Diesel Generator Sets with Six New 50-Hz Standby Power Ratings up to 3,500 kVA

 

For Worldwide Release: February 24, 2020
Release Number: EEPR0120 

DEERFIELD, IL – Caterpillar Inc. today announced the introduction of six new 50-Hz standby ratings that deliver industry-leading power density while helping to reduce overall site preparation, transportation, installation and maintenance costs.  

Caterpillar now offers the Cat® 3516E diesel generator set with the following 50-Hz standby power ratings and emissions thresholds:

  • three ranging from 3,000 kVA to 3,500 kVA that provide certification to U.S. EPA Tier 2 emissions standards;
  • two from 3,000 kVA to 3,250 kVA that offer nitrogen oxide (NOx) emissions under 2,000 mg/Nm3; and
  • one low-NOx 3,500 kVA rating for regulated environments and applications.

The Cat® 3516E diesel generator set with the 3,500 kVA rating offers an 8,800-kg (19,400-lb) weight reduction over a leading competitive product offering the same power output, while occupying 15% less floor space.

With the launch of these new power ratings, Caterpillar now offers diesel generator sets with industry-leading power densities that range from 850 kVA to 3500 kVA.

“Customers evaluate standby power solutions across many dimensions beyond power output and price,” said Bart Myers, general manager for Caterpillar Large Electric Power Solutions. “These new power ratings demonstrate Caterpillar’s continued investment in our engine and power technologies to give our customers superior product value accompanied by our unmatched design and dealer support.”

Cat 3516E generator sets are designed to meet the NFPA power restoration requirement for Level 1 systems and accept 100 percent block load in one step. They meet ISO 8528-5 G3 requirements for steady state and load acceptance.

The new power ratings are available with a low-, medium- or high-voltage frame alternator that enables quick load acceptance through exceptional motor starting capabilities. This feature eliminates the need to oversize the generator set due to motor starting requirements.

The Cat 3516E generator set utilizes the field-proven Cat ADEM™ A5 engine control module (ECM). This module seamlessly integrates all engine functions including ignition, governing and air-fuel ratio control for optimal performance while protecting the engine.

Caterpillar delivers innovative power systems engineered for durability, reliability and value. The company offers worldwide product support, with parts and service available globally through the Cat authorized service and dealer network. In addition, dealer service technicians are trained to service every aspect of Cat equipment.

For more information, visit www.cat.com/powerdensity or e-mail Electric_Power@cat.com

 

 

 

Download High Resolution Image

Or 
Contact Bob Chase at bchase@gelia.com
 
of

Cat® 3516E Diesel Generator Set

Product & Service News

See the latest product and engine announcements from Caterpillar.

See the Latest News

 

# # #

About Caterpillar

Since 1925, Caterpillar Inc. has been helping our customers build a better world – making sustainable progress possible and driving positive change on every continent. With 2019 sales and revenues of $53.8 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. Services offered throughout the product life cycle, cutting-edge technology and decades of product expertise set Caterpillar apart, providing exceptional value to help our customers succeed. The company principally operates through three primary segments - Construction Industries, Resource Industries and Energy & Transportation - and provides financing and related services through its Financial Products segment. For more information, visit caterpillar.com. To connect on social media, visit caterpillar.com/social-media.

# # #

CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

©2020 Caterpillar
All Rights Reserved

 

Press Inquiries

Bob Chase
Gelia
Tel: +1 716-629-3230
bchase@gelia.com

Anne O’Boyle
Caterpillar Inc.
Tel: +028 9049 5269
OBoyle_Anne@cat.com

Reader Requests

Caterpillar Inc.
Large Electric Power Business
P.O. Box 0610
Mossville, IL 61552-0610