If you already have an existing account with another Cat App, you can use the same account to sign in here.
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
For Worldwide Release: January 30, 2013
Release Number: CMPS13PR1
Caterpillar Incorporated and FPT Industrial S.p.A. announce an agreement in the field of marine pleasure craft engines. According to the new agreement, combining the vast marine know-how of Caterpillar and the leading edge technology of FPT Industrial, the new Cat C8.7 and Cat C12.9, with a displacement of 8.7 and 12.9 liters respectively, will offer yacht manufacturers a broad array of horsepower ratings ranging from 650 to 1000 mhp. In order to meet customers’ unique requirements, each engine will be offered in several different configurations; all will conform to Tier 3 emissions regulations.
Caterpillar has been a mainstay in marine propulsion for over seventy years, while FPT Industrial is a firm that can trace its roots back to the turn of the twentieth century. The new venture between the two revered engine manufacturers will provide unmatched value to customers, beginning with the sophisticated design of the engines, continuing with the ease of installation, and culminating with the serviceability of the new power plants. FPT Industrial’s latest technological developments include implementing second-generation common rail fuel injection and advanced and innovative air handling techniques which together allow an extremely high power density and generous amounts of low-end torque. The new engines’ compact envelope creates a myriad of new possibilities, all of which result in remarkable performance gains. For example, a pair of the new 1000 mhp engines can now be installed in a hull design which previously was limited with size constraints to engines of a much lower rating. Servicing of the new engines is straightforward thanks to right- or left-hand service options, and of course the new product is backed by Caterpillar’s world renowned dealership network.
The pairing of the two diesel engine manufacturers seems to be the perfect match-- FPT’s innovations and developments combined with Caterpillar’s vast marine experience and global dealer presence will grant customers fuel efficiency while at the same time providing best-in-class power, torque, and load response.
# # #
Note to Editors: Caterpillar rolls-out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.
Jenna Janik
Tel: +1.713.895.1449
Janik_Jenna_E@cat.com