Caterpillar Introduces New 3,000 kW Node for 60 Hz Standby and Mission Critical Applications

For Worldwide Release: August, 2020 

DEERFIELD, IL – Caterpillar Inc. today announced the availability of a new 3,000 kW power node for the Cat® 3516E diesel generator set in 60 Hz standby and mission critical applications. The launch of the uprated Cat 3516E generator set further expands Caterpillar’s industry leadership in diesel generator sets with high power densities that are designed to deliver the lowest owning and operating costs in their class.

Providing certification to U.S. EPA Tier 2 emissions standards, the Cat® 3516E diesel generator set offers a 19,900-lb (9,000-kg) weight reduction over a leading competitive product offering the same power output, while occupying 11 percent less floor space. These features help to reduce overall site preparation, transportation, cranage, building support, and other installation costs for customers.

The Cat 3516E diesel generator set is available with an optional high-ambient radiator that enables the production of full power in ambient temperatures of up to 131 degrees Fahrenheit (55 degrees Celsius) without derating.

Cat 3516E diesel generator sets are designed to meet the NFPA power restoration requirement for Level 1 systems and accept 100 percent block load in one step. They meet ISO 8528-5 G3 requirements for steady state and load acceptance.

The new power ratings are available with a low-, medium-, or high-voltage frame alternator that enables quick load acceptance through exceptional motor starting capabilities. This feature eliminates the need to oversize the generator set due to motor starting requirements.

The Cat 3516E generator set utilizes the field-proven Cat ADEM™ A5 engine control module (ECM). This module seamlessly integrates all engine functions including ignition, governing, and air-fuel ratio control for optimal performance while protecting the engine.

Caterpillar delivers innovative power systems engineered for durability, reliability, and value. The company offers worldwide product support, with parts and service available globally through the Cat authorized service and dealer network. In addition, dealer technicians are trained to service every aspect of Cat equipment.

For more information, visit www.cat.com/powerdensity or e-mail Electric_Power@cat.com.

of

Cat® 3516E diesel generator set offering 3,000 kW for standby and mission critical applications

Product and Services News

See the latest product and engine announcements from Caterpillar.

See the Latest News

 

###

About Caterpillar

Since 1925, Caterpillar Inc. has been helping our customers build a better world – making sustainable progress possible and driving positive change on every continent. With 2019 sales and revenues of $53.8 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines, and diesel-electric locomotives. Services offered throughout the product life cycle, cutting-edge technology and decades of product expertise set Caterpillar apart, providing exceptional value to help our customers succeed. The company principally operates through three primary segments - Construction Industries, Resource Industries and Energy & Transportation - and provides financing and related services through its Financial Products segment. For more information, visit caterpillar.com. To connect on social media, visit caterpillar.com/social-media.

© 2020 Caterpillar. All Rights Reserved. CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, ADEM, "Caterpillar Corporate Yellow", the "Power Edge" and Cat “Modern Hex” trade dress as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

Press Inquiries

Bob Chase
Gelia
Tel: +1 716-629-3230
bchase@gelia.com

Sarah Pullen
Caterpillar Inc.
Tel: +1 309-675-1513
Pullen_Sarah_C@cat.com

 

Reader Requests

Caterpillar Inc.
Electric Power Division
P.O. Box 0610
Mossville, IL 61552-0610