If you already have an existing account with another Cat App, you can use the same account to sign in here.
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
Hamburg, Germany - Caterpillar Marine will unveil new power ratings for the Cat® C175 propulsion engine for commercial vessels at the 2014 SMM Exhibition, held September 9 -12 in Hamburg, Germany. Designed specifically as a high speed power solution for commercial applications including ocean going and harbor tugs, the C175-16 propulsion engine is now available with ratings of 2239 bkW - 2550 bkW @ 1800 rpm. The new ratings extend Caterpillar Marine’s high-speed engine power range beyond the company’s already industry-leading 3516C HD engine. Cat C175 engine platforms with the new ratings are available to order now from the global Cat dealer network.
“Designed to improve total vessel profitability by providing durability with unmatched power output, the C175 offers ample benefits to our tug and salvage customers as a durable, high performance performer,” Nathan Kelly, Caterpillar Marine product definition engineer noted. “Additionally, the platform also offers improved serviceability, providing more access to the cylinder heads and valve train components.”
Ideal for large, high speed commercial vessels, the C175 engine utilizes proven ACERTTM technology to optimize turbocharging and aftercooling. Efficient combustion reduces engine wear and maximizes fuel, driving the C175-16 to pull the maximum amount of energy from each injection event. The engine also features the Cat common rail fuel system enabling low emissions at all levels and requires no aftertreatment to comply with regulations. In addition to an 1,000-hour oil change interval, thermo-laminated heat shields save time and money during service.
With a bore of 175 mm (6.9 in) and a stroke of 220 mm (8.66 in), the C175-16 is highly efficient while providing increased propulsion output in a high speed engine platform. Additional features include:
Cat Marine power and propulsion solutions are backed by the worldwide Cat dealer network with trained technicians to ensure service support is never out of reach. Visit us at SMM Hamburg in Hall A4 at Booth #204. For more information on Caterpillar Marine, visit www.marine.cat.com. For information on Cat Propulsion products, visit www.catpropulsion.com. Follow us on Facebook: www.facebook.com/caterpillarmarine and Twitter @catmarineglobal using #catatsmm.
# # #
Caterpillar Marine, with headquarters in Hamburg, Germany, groups all the marketing and service activities for Cat and MaK™ marine diesel, dual fuel and gas power and propulsion systems within Caterpillar Inc. The organisation provides premier power solutions in the medium- and high-speed segments with outputs from 93 to 16,800 kW in main propulsion and 10 to 16,100 kWe in marine generator sets as well as a comprehensive portfolio of propulsion solutions. The sales and service network includes more than 2,100 dealer locations world-wide dedicated to support customers in ocean-going, commercial marine and pleasure craft wherever they are.
More information is available at: MARINE.CAT.COM/pr
For nearly 90 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent. Customers turn to Caterpillar to help them develop infrastructure, energy and natural resource assets. With 2013 sales and revenues of $55.656 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. The company principally operates through its three product segments - Resource Industries, Construction Industries and Energy & Transportation - and also provides financing and related services through its Financial Products segment. For more information, visit caterpillar.com. To connect with us on social media, visit caterpillar.com/social-media.
Press Inquiries
Jenna Janik Marcoux
Phone: +1 713 895 1449
Marcoux_Jenna_J@cat.com