If you already have an existing account with another Cat App, you can use the same account to sign in here.
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
December, 2021
Houston, TX –Caterpillar Oil & Gas is pleased to announce an increase to the already great fuel tolerance of the Cat® G3600 with ADEM A4 engine line. Today Caterpillar Oil & Gas released the updated technical data sheet for a flat Fuel Usage Guide (FUG) allowing the engines to run at full rating down to a Cat Methane Number (MN) 32.
“We are once again expanding the fuel tolerance of the 3600 A4 line giving customers a wider range of fuels in which they can operate without having to take a derate on their engine,” said Bill Mermoud, market development consultant at Caterpillar.
The G3600 A4 provides users with an increase of over 5.5% in horsepower rating and allows for operation over the broad range of fuels found in today’s compression applications. “Further horsepower increases are possible when operators take advantage of the engine’s ambient based rating (ABR) capability. ABR allows more horsepower to be available from the G3600 A4, be it seasonally or daily as local temperatures drop and provide cooler inlet air to the engine.” said Mermoud.
For decades, Caterpillar Oil & Gas has powered the gas compression industry with industry-leading gas-fuelled engines, including the legendary Cat G3500 and G3600 product platforms. Built using the proven Cat diesel designs, Cat gas-fuelled engines have stood up to the most demanding natural gas applications for more than fifty years, delivering legendary reliability and durability.
The updated flat FUG can be located in the Caterpillar Gas Engines Ratings Pro which is now available online at Cat.com/GERP.
ABOUT CATERPILLAR OIL & GAS
Caterpillar Oil & Gas, Caterpillar Inc.’s oil and gas division with headquarters in Houston, Texas, consolidates all the sales and service activities for Cat oil and gas power solutions. Since the 1930s, Caterpillar has manufactured engines for the oilfield and today provides premier power solutions with outputs from 31 to 16,000 kW. The sales and service network includes more than 2,100 dealer locations world-wide dedicated to support customers in the drilling, production, well service and gas compression segments. More information is available at: www.cat.com/oilandgas.
ABOUT CATERPILLAR
For over 90 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent. Customers turn to Caterpillar to help them develop infrastructure, energy and natural resource assets. With 2015 sales and revenues of $47.011B, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. The company principally operates through its three product segments - Resource Industries, Construction Industries and Energy & Transportation - and also provides financing and related services through its Financial Products segment. For more information, visit caterpillar.com. To connect with us on social media, visit caterpillar.com/social-media.
©2016 Caterpillar
All Rights Reserved
Press Inquiries
Sarah Pullen
Phone: +1 309 675 1513
Jenna Janik Marcoux
Phone: +1 713 895 1449