If you already have an existing account with another Cat App, you can use the same account to sign in here.
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
Starting in early 2024, the advanced hydrogen-hybrid project will leverage the versatile new Cat® C13D engine platform.
For Worldwide Release November 20, 2023
Caterpillar today announced the launch of a three-year program to demonstrate an advanced hydrogen-hybrid power solution built on its new Cat® C13D engine platform.
Starting in the first quarter of 2024, Caterpillar will develop a transient-capable system for off-highway applications. The project will demonstrate how state-of-the-art control systems and electric-hybrid components can help hydrogen-fueled engines meet or exceed the power density and transient performance of traditional diesel engines.
Caterpillar will serve as the prime contractor on the project, providing engine research and development as well as system integration. As the project progresses, other industry and academic collaborators will be brought into the program to provide additional specialist expertise. The initiative will be delivered at Caterpillar facilities in Chillicothe, IL and San Antonio, TX.
With research commencing in 2024, the project is supported and partially funded by the U.S. Department of Energy’s (DOE) Vehicle Technologies Office (VTO) through the Office of Energy Efficiency and Renewable Energy (EERE). It is included among 45 projects across 18 states and Washington, D.C., receiving funding to advance research, development, demonstration, and deployment in several areas critical to reducing greenhouse gas (GHG) emissions in the transportation sector.
The hydrogen-hybrid power demonstration project is the latest in a series of initiatives that builds upon Caterpillar’s 35 years of enterprise experience in hydrogen fuels.
“Every off-highway application has its own unique duty cycles, lifecycle demands and performance expectations, and this complexity is driving the development of a wide range of power solutions for the energy transition,” said Steve Ferguson, senior vice president Caterpillar Industrial Power Systems. “One size does not fit all, which is why we’ve engineered flexibility into the C13D engine to serve as our platform of the future.”
Future Fuel Readiness of Caterpillar’s Latest Engine Platform
Caterpillar’s hydrogen-hybrid demonstration project leverages the performance, packaging, and fuel flexibility engineered into the new 13-liter Cat C13D engine platform.
Unveiled at the CONEXPO-CON/AGG 2023 construction exhibition in March, diesel-powered versions of the Cat C13D engine offer eight power ratings from 456 to 690 hp (340 to 515 kW) with up to 3,200 Nm of peak torque. It provides up to a 20% increase in power and up to 25% more low-speed torque over the previous generation of Cat diesel engines in its power class.
The inline, six-cylinder Cat C13D enables the use of renewable liquid fuels such as 100% HVO, B100 Distilled Biodiesel, and even up to B100 Standard Biodiesel by working with the local Cat dealer*. In addition to using hydrogen, its core architecture is designed for the future development of spark-ignited natural-gas capabilities.
Available for early OEM pilots in 2025 and scheduled for production in 2026, the Cat C13D engine is targeted for a wide range of off-highway equipment, including rock crushers, screeners, and grinders; trenchers; agriculture tractors, harvesters, self-propelled sprayers and woodchippers; material-handling equipment; and large industrial pumps.
For more details on Caterpillar’s comprehensive range of solutions supporting a lower carbon future, visit the Industrial Power Sustainability area.
*To preserve the performance and integrity of the engine while reducing the risk of downtime or failure, fuels must meet the specifications and characteristics described in Caterpillar’s official fluids guideline documents found on cat.com.
About Caterpillar
With 2022 sales and revenues of $59.4 billion, Caterpillar Inc. is the world’s leading manufacturer of construction and mining equipment, off-highway diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. For nearly 100 years, we’ve been helping customers build a better, more sustainable world and are committed and contributing to a reduced-carbon future. Our innovative products and services, backed by our global dealer network, provide exceptional value that helps customers succeed. Caterpillar does business on every continent, principally operating through three primary segments – Construction Industries, Resource Industries and Energy & Transportation – and providing financing and related services through our Financial Products segment. For more information, visit caterpillar.com. To connect with us on social media, visit caterpillar.com/social-media.
CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.
©2023 Caterpillar
All Rights Reserved
Press Inquiries for Cat Industrial Power Systems: