If you already have an existing account with another Cat App, you can use the same account to sign in here.
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
Hamburg Germany – Caterpillar Marine is pleased to announce MaK™ diesel electric propulsion (DEP) solutions have been selected to power four Maersk Supply Services (MSS) newbuilds to be constructed by COSCO (Dalian) Shipyards. Each vessel will be equipped with 4x MaK M 32 E generator sets with a power output of 4,400 kW each and 2x MaK 8 M 20 C at 1440 kW each. The new M 32 E engine solutions boast an increased power rating of 550 kW per cylinder @ 720 and 750 rpm, with total output ranging from 3,300 kW for the six cylinder configuration to 4,950 kW for the nine cylinder configuration. Additionally, the M 32 E generator sets feature the recently-introduced constant speed part load kit for the M 32 E, providing fuel savings up to 10 g/kWh with a 3x33% load step capability.
“We’re pleased the high performance, part-load optimized M 32 E power solutions have been selected for the Maersk subsea service vessels,” Alexander Kohse, Caterpillar Marine offshore segment manager noted. “The vessels will benefit from the lowest possible fuel consumption while operating in part load range but still deliver the reliable MaK power in full throttle.”
Designed to carry out subsea cable laying, installation and maintenance, the subsea service vessels will be rated for operations in water up to 3,000 meters. The MaK engines will be delivered to the shipyard with enhanced safety offerings, such as a high standard exhaust cladding design for surface temperature control. Offering both 720 and 750 rpm, the higher power output M 32 E is ideal for diesel electric propulsion and auxiliary power applications complementing the multi-engine concepts which are typical for the offshore market. Compared to previous solutions the new design allows to substantially reducing the footprint of the generator set.
Besides the higher engine power density, the length and weight of the package has been reduced by more than 15%, without compromising reliability, durability, vibrations and structural borne noise. A seamless integration of the control system into the vessel electronics is ensured by the new modular alarm and control system (MACS). With MACS, the M 32 E can as well be perfectly integrated with the proven Cat® high speed engines in mixed engine rooms by using common Cat Electronics components like the legendary Cat ADEM™ A4 engine control module.
Cat marine power and propulsion solutions are backed by the worldwide Cat dealer network with trained technicians to ensure service support is never out of reach. Visit us at the International Workboat Show, December 3rd – 5th in New Orleans, Louisiana, booth #2802. For more information on Caterpillar Marine, visit www.marine.cat.com. For information on Cat Propulsion products, visit www.catpropulsion.com. Follow us on Facebook: www.facebook.com/caterpillarmarine and Twitter @catmarineglobal during the show using #CatWBS.
# # #
Caterpillar Marine, with headquarters in Hamburg, Germany, groups all the marketing and service activities for Cat and MaK™ marine diesel, dual fuel and gas power and propulsion systems within Caterpillar Inc. The organisation provides premier power solutions in the medium- and high-speed segments with outputs from 93 to 16,800 kW in main propulsion and 10 to 16,100 kWe in marine generator sets as well as a comprehensive portfolio of propulsion solutions. The sales and service network includes more than 2,100 dealer locations world-wide dedicated to support customers in ocean-going, commercial marine and pleasure craft wherever they are.
More information is available at: MARINE.CAT.COM/pr
For nearly 90 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent. Customers turn to Caterpillar to help them develop infrastructure, energy and natural resource assets. With 2013 sales and revenues of $55.656 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. The company principally operates through its three product segments - Resource Industries, Construction Industries and Energy & Transportation - and also provides financing and related services through its Financial Products segment. For more information, visit caterpillar.com. To connect with us on social media, visit caterpillar.com/social-media.
Press Inquiries
Jenna Janik Marcoux
Phone: +1 713 895 1449
Marcoux_Jenna_J@cat.com