Caterpillar continues to be successful in MaK™ Dual Fuel engine retrofits & supplies complete gas system for Fure West Tanker
Hamburg Germany – Building on the success of recent MaK diesel engine dual fuel retrofit conversions, Caterpillar Marine is currently underway on another dual fuel engine retrofit conversion onboard the 472 foot Fure West tanker, owned by Furetank Rederi A/B. The MaK™ M 43 C diesel engine onboard the tanker will be retrofitted in hull to the 7 cylinder M 46 dual fuel platform, with each cylinder offering 900 kW of rated power. Additionally, Caterpillar is also supplying the complete gas system for the tanker, including bunker stations, 2x LNG tanks measuring 4.15 meters by 24 meters and the vaporizer.
This project, backed by the European Union and developed with the Zero Vision Tool, will mark the second MaK engine dual fuel retrofit. In 2014, Caterpillar successfully completed the dual fuel engine retrofit conversion on the Anthony Veder Coral Anthelia LNG carrier. “We’re pleased to continue to build upon our successful track record of dual fual conversions in the commercial marine industry and offer an increased scope of supply to our customers,” Finn Vogler, Caterpillar Marine senior engineer noted. “We have a market-ready technology available that our commercial marine customers can be completely confident in and after our success onboard the Coral Anthelia, we have seen the demand for MaK dual fuel solutions increase substantially.”
With a bore of 460 millimeters and stroke of 610 millimeter, the M 46 dual fuel engine was designed for electric drive propulsion systems as well as mechanical propulsion systems. Although designed for unlimited operation on LNG, marine diesel oil and heavy fuel oil, the M 46 DF will reach industry-leading efficiency in gas mode. The M 46 DF was strategically engineered to allow for the retrofitting of current M 43 C engines. Additionally, existing M 32 E engines can be retrofitted to the MaK M 34 DF dual fuel platform. As a result of the synergies between the two platforms, Caterpillar can perform in hull retrofit conversions without having to move the engine block or perform extensive machining. For the Fure West conversion, Cat dealer Pon Power had a significant role in the project. “We’re able to differentiate our solutions in the market by offering a collaborative partnership with our dealers to ensure the retrofit conversions are completed in an expedited manner and with a reduced number of parties involved as a result of our ability to provide the complete gas system for a vessel as well,” Vogler noted.
Cat marine power and propulsion solutions are backed by the worldwide Cat dealer network with trained technicians to ensure service support is never out of reach. For more information on Caterpillar Marine, visit www.marine.cat.com. For information on Cat Propulsion products, visit www.catpropulsion.com. Follow us on Facebook: www.facebook.com/caterpillarmarine and Twitter @catmarineglobal.