Ashland, Kentucky – When long-time customer Marathon Petroleum wanted to repower inland river towboats, they turned to their trusted Cat® dealer Boyd Cat to get the job done. Marathon had installed Cat 3606 engines on the inland waterways vessels in the early 1990s and twenty years later was ready to repower three towboats with the successor to the 3600 engine series, the Cat C280. Starting in December 2013, Boyd Cat worked with Marathon to repower the three vessels with Cat C280-6 engines, each rated at 2548 bhp @ 900 rpm.
“Marathon Petroleum has been a proud Cat customer for decades and had great success with the reliability and durability of the Cat 3606 engines since the initial installation of the engines,” Neilly Allen, Boyd Cat marine account manager noted. “They were impressed with the long overhaul intervals and were eager to repower their vessels with the C280 engines, which have the perfect speed and power fit for their applications on the inland rivers.”
Manufactured in Lafayette, Indiana, Cat C280 engines incorporate 30 years of proven component reliability and durability from the legendary Cat 3600 platform series with a sophisticated, yet well-proven, modern electronic fuel injection system. Cat C280 marine engines are available in continuous and maximum continuous ratings at 900 and 1000 rpm and in 6, 8, 12, and 16 cylinder configurations The advanced ADEM™ A3 electronic control system enables the C280 engines to work smarter and harder. The rugged and durable C280 engines provide customers with low owning and operating costs, with overhaul intervals running as long as 40,000 hours. “At Whayne, our customers have found the C280 delivers on the same Cat brand promise as the 3606 engines, which developed a long-standing reputation on the waterways as a reliable workhorse,” Allen noted. “With the increasing demands for the C280 platform on inland waterway applications, we’ve become incredibly proficient at completing comprehensive repowers quickly to get our customers’ vessels back on the water.”
Cat marine power and propulsion solutions are backed by the worldwide Cat dealer network with trained technicians to ensure service support is never out of reach. For more information on Caterpillar Marine, visit www.marine.cat.com. Follow us on LinkedIn: www.linkedin/showcase/caterpillar-marine and Facebook: www.facebook.com/caterpillarmarine
About Caterpillar Marine
Caterpillar Marine, with headquarters in Hamburg, Germany, groups all the marketing and service activities for Cat® and MaK marine diesel, dual fuel and gas power and propulsion systems within Caterpillar Inc. The organization provides premier power solutions in the medium- and high-speed segments with outputs from 93 to 16,800 kW in main propulsion and 10 to 16,100 kWe in marine generator sets as well as a comprehensive portfolio of propulsion solutions. The sales and service network includes more than 2,100 dealer locations world-wide dedicated to support customers in ocean-going, commercial marine and pleasure craft wherever they are. More information is available at: www.cat.com/marine
About Caterpillar
For more than 90 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent. Customers turn to Caterpillar to help them develop infrastructure, energy and natural resource assets. With 2018 sales and revenues of $54.722 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. The company principally operates through its three primary segments - Construction Industries, Resource Industries and Energy & Transportation - and also provides financing and related services through its Financial Products segment. For more information, visit www.cat.com. To connect on social media, visit caterpillar.com/social-media.
© 2020 Caterpillar. All Rights Reserved. CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, "Caterpillar Yellow", the "Power Edge" and Cat “Modern Hex” trade dress as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.
Trade Press Inquiries
Danielle Wills
Wills_Danielle@cat.com