If you already have an existing account with another Cat App, you can use the same account to sign in here.
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
NEW PREMIUM OIL FILTRATION SYSTEM FOR POWER END LUBRICATION
Houston, Texas – The leading cause of premature power end failure is contamination of the lubrication oil. To address this issue Caterpillar has released a premium Oil Filtration system for the Power End Lubrication as an installed standard attachment.
The Cat® Well Stimulation Pump Power End Lube Oil Filtration allows oil to be cleaned with the specifications that Caterpillar recommends. By integrating industry leading filters from the TH55 transmission into the power end filtration system, Caterpillar provides world class filtration to power ends, as well as parts commonality with the transmission of choice for well stimulation customers.
The oil filtration system is available on every Power End Only, Complete Pump, and Configurable Pump horsepower.
One benefit of the system is simplified maintenance, as it is capable of being mounted on the power end itself, allowing for rapid filter changes. Meticulously designed, the filtration system provides its greatest benefit of limiting contamination downstream. Now, there is less chance of debris being introduced from intermediate components.
Another convenience of the system is the ability to use the same tools for transmission filter changes.
Two additional features of the system include an integrated bypass sensor and sampling ports both upstream and downstream of the filter to allow for a consistent oil sampling process. In conjunction with a Scheduled Oil Sampling (SOS) program, this allows extended oil change intervals while ensuring satisfactory oil cleanliness. The oil filtration system is fully integrated with the Pump Electronic Monitoring System (PEMS), which provides oil pressure, oil temperature, and filter differential pressure data via J1939 standard.
Available now, the new system is compatible with and recommended for retrofit of already shipped Cat power ends.
About Caterpillar Oil & Gas
Caterpillar Oil & Gas, Caterpillar Inc.’s oil and gas division with headquarters in Houston, Texas, consolidates all the sales and service activities for Cat oil and gas power solutions. Since the 1930s, Caterpillar has manufactured engines for the oilfield and today provides premier power solutions with outputs from 31 to 16,000 kW. The sales and service network includes more than 2,100 dealer locations world-wide dedicated to support customers in the drilling, production, well service and gas compression segments. More information is available at: www.cat.com/oilandgas.
About Caterpillar
For over 90 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent. Customers turn to Caterpillar to help them develop infrastructure, energy and natural resource assets. With 2016 sales and revenues of $38.5 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. The company principally operates through its three product segments - Construction Industries, Resource Industries and Energy & Transportation - and also provides financing and related services through its Financial Products segment. For more information, visit caterpillar.com. To connect with us on social media, visit caterpillar.com/social-media.
©2018 Caterpillar
All Rights Reserved
Press Inquiries
Danielle Wills