Mining

Cat® 797F Mining Truck Proven in Tier 4 Final Configuration

For Release Worldwide: March 2019 
Release Number: 128PR19

The Cat® 797F large mining truck is now available in a fuel-efficient configuration that meets U.S. EPA Tier 4 Final emissions standards. Through more than 16,000 hours of successful pilot machine operation and 100,000 hours of production truck operation in Tier 4 configuration, the system has proven its ability to deliver strong performance and greater fuel efficiency compared to the Tier 2 797F in most applications.

The 797F Tier 4 Final is equipped with an exhaust aftertreatment system featuring selective catalytic reduction (SCR), which uses diesel exhaust fluid (DEF) to lower NOx emissions.  This Cat emissions platform is proven through more than 20 million operating hours in the field. To maintain superior reliability, the 797F aftertreatment system uses less than 11 percent new content. Designed for easy serviceability with readily accessible components, the modular aftertreatment system is aligned with truck preventive maintenance intervals to maintain high availability.

The best-selling truck in the 400-ton (363-tonne) size class, the 797F is powered by the 4000-hp (2 983-kW) Cat® C175-20 engine, available with optimized fuel maps for customers focused on the lowest fuel burn, Tier 2 equivalent rating, and now Tier 4 Final. Known for delivering class-leading payload and speed-on-grade performance, the 797F delivers the same production performance in Tier 2 and Tier 4 Final configurations.

Beyond offering similar performance, the Tier 4 Final 797F reduces total specific fluid consumption costs (fuel plus DEF) in most applications. Lower fuel burn results in longer engine life and lower repair costs.

Field evaluations of the low-emissions 797F included a wide range of applications, including oil sands, deep pit copper, iron ore and coal. The trucks exceeded production targets and demonstrated strong engine performance in all applications, including sites with extreme ambient temperatures as well as some with altitudes greater than 16,000 ft (4 877 m).

For more information about the Cat 797F large mining truck, contact the local Cat dealer or visit: www.cat.com 

 

Cat 797F Tier 4 Final Specifications

Engine

Cat C175-20

Gross Power (SAE J1995)

4,000 hp (2 983 kW)

Net Power (SAE J1349)

3,793 hp (2 828 kW)

Target Gross Machine Weight

1,375,000 lb (623 690 kg)

Nominal Payload Capacity

400 tons (363 tonnes)

# # #

CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

VisionLink is a trademark of Trimble Navigation Limited, registered in the United States and in other countries.

©2019 Caterpillar. All Rights Reserved.

Press Inquiries

Caterpillar Trade Press Media Representatives

Americas

Sharon Holling: Holling_Sharon_L@cat.com

Johanna Kelly: Kelly_Johanna_L@cat.com

Europe, Africa, Middle East

Francine Shore: Shore_Francine_M@cat.com

 

Reader Requests

www.cat.com/requestCatinfo